Solutions Partner Catalog Keysight Technologies & TOYO Corporation EMC Measurements

Brochures

About TOYO Corporation

TOYO Corporation, as an expert in measurement technology, has been proactively breathing fresh life into the sunrise industry such as energy and environment, along with its mainstream business including electromagnetic interference measurement and communication measurement. Striving for a name trusted in the market innovation technology, not only a measurement technology provider, we, at TOYO, redouble our efforts to expand the laboratories, impart technical knowledge, improve the training facilities and enrich technical training for employees. In recent years, TOYO has been delivering carefully needs-matched solutions to each customer through self-developed system products and will be committed to promptly catering to the demand for technological innovation with a reinforced development group.

Overview

With electronic devices going digital and mobile through high-density implementation, it is getting more difficult to isolate noise sources, and more cost- and time-consuming to implement appropriate EMI remedies against them.

TOYO EP7 software, which is designed for EMI evaluation measurements, collects and saves a greater-than-ever amount of data on the complicated noises emitted by such digital devices, thereby detecting noises that could not be captured before through automated measurements with enhanced speed and reliability. Furthermore, the EP7 has reinforced functionality for the post measurement evaluation and analysis of DUT through multi-angle visualization of an enormous amount of measurement data among other means.

TOYO EP9 software, which is meant for automobile EMI measurements, has been developed to be compliant with diversifying international and automobile manufacturers’ own standards. The EP9 adopts a matrix system that allows users to narrow down measurement conditions simply by selecting a standard and a transducer.

Immunity Test Software

Overview

TOYO IM5 series software, which performs automated immunity testing, has been developed to evaluate the immunity of electronic devices against electromagnetic interference. The IM5’s capability to automatically control the instruments required for immunity testing (e.g. a signal generator, power amplifier system, electric-field strength meter, power meter, and antenna mast) allows any users to conduct EMI measurements in an efficient and secure manner, as well as to output measurement data to a printer and to save such data on a hard disk drive.

With an error detection option installed, the IM5 monitors the DUT being subjected to an immunity test and, if any limit setting is exceeded, detects it as an error. TOYO VI5 series software, which also is for automated immunity testing, has been developed specifically to test automobiles for their immunity against electromagnetic interference. As is the case with all other TOYO EMC/EMI software applications, the VI5 is constantly updated and upgraded to better serve customer needs, an example of which is the implementation of an error detection function utilizing CAN/LIN bus monitor and image recognition.