Data Loggers | Keysight Equipment Screenshot to Test Scalability

Data Loggers: The Answer to Test Scalability Bottlenecks


Key takeaways:

For rapid time-to-market and maximum customer satisfaction, engineers must be able to thoroughly test electronic systems as quickly and productively as possible.

Data loggers facilitate rapid, convenient testing of large numbers of devices. In this blog post, learn more about data loggers, find out which industries use them, and understand what makes them advantageous for your electronics testing.

What is a data logger?

Data Loggers | What Is a Data Logger? | Testing With Data Logger Versus Multiple Instruments Illustration

Figure 1. Testing with data logger versus multiple instruments

The term "data logger" can refer to several things in the electronics industry. In general, a data logger is a device or software that measures some electrical or physical parameters and stores them. However, data loggers vary significantly in form and function. Below are four commonly used types of data loggers:

  1. Specialized instrument for data logging during testing: In lab and production environments, a data logger can refer to a data acquisition (DAQ) instrument that can simultaneously measure electrical and physical parameters from a large number of test points across one or more devices under test (DUTs). For a complex DUT that requires a variety of parallel measurements, connecting a single data logger is more convenient and faster than wiring up dozens of multimeters and other instruments, as shown in the above illustration.
  2. Software-based data logging during testing: The term "data logger" can also refer to the functionality of measurement data logging provided by DAQ software. For example, the PathWave BenchVue suite includes a data logging feature for DAQ systems.
  3. Built-in data logging in non-DAQ instruments: Sometimes, data logging is a built-in secondary capability of some non-DAQ instruments like the Keysight N6705C power analyzer.
  4. Portable environmental monitoring device: A data logger can also refer to a portable battery-powered environmental monitoring device used for optimal operations and maintenance in industries like food storage, life sciences, aerospace, and geoscience. These industries use a variety of devices like temperature data loggers, humidity data loggers, pressure data loggers, carbon dioxide detectors, and more. Such data loggers can run for weeks or even months due to a long battery life. The recorded data is regularly uploaded to a monitoring center over ethernet, Wi-Fi, or Bluetooth.

In this blog, we focus on the first two types of data loggers — instruments or software for simultaneous measurements in lab, production, and end-of-line test setups.

How is a data logger different from other data acquisition instruments?

A data logger optimizes bench testing and streamlines production testing where hundreds of DUTs must be automatically verified every day. In this, data loggers are like other DAQ systems.

However, unlike typical data acquisition systems, a data logger generally (but not necessarily) carries the connotations below:

What are the key applications of data loggers across different industries?

Data loggers support a high number of simultaneous measurements and a wide range of electrical and physical parameters.

These benefits make them incredibly useful in quality-sensitive industries as outlined below.

Automotive

Data Loggers | Data Loggers in Automotive Testing | Testing Comfort, Perfomance, Monitoring and Stress

Figure 2. Data loggers in automotive testing

Data loggers are used for testing components and ensuring compliance with automotive standards and regulations. Some specific uses are explained below:

Aerospace and defense

Data loggers are extensively used for testing electronic and electromechanical components in aerospace and defense systems. Uses include:

For example, the National Aeronautics and Space Administration (NASA) has used Keysight's data loggers in spacecraft electric propulsionresearch to measure voltages, currents, fluid flow, and power for durability tests spanning hundreds of hours.

Semiconductor engineering

Since integrated circuits have hundreds to thousands of input/output pins and other test points, integrated DAQs as well as standalone data loggers are used for simultaneous measurements during on-wafer testing, post-silicon validation, and package testing.

For example, NASA has tested copper-wire-bonded semiconductorpackaging for space applications using Keysight data loggers to measure component voltages and current draws as well as power supply voltages and component temperatures.

Electronics manufacturing

Data loggers are extensively used for:

What are the advantages of using data loggers over manual data recording?

Manual data recording involves wiring up instruments like digital multimeters and power analyzers to a DUT to measure various parameters. However, as the number of measurements, instruments, or DUTs increases, this approach becomes increasingly inconvenient, inefficient, and expensive.

Data loggers prevent those problems and bring additional benefits as explained below.

High scalability

Data loggers are designed for simultaneous measurements from hundreds of test points. They delegate the measurements to add-on modules like multiplexers that support hundreds of measurement channels. Many such add-on modules can be added to data loggers to expand the number of channels.

Manually connecting, configuring, and synchronizing dozens of multimeters and other instruments one by one is very time-consuming. While wiring is still required for data loggers, configuration and synchronization can be finished quickly.

High-speed measurements

Data loggers can scan hundreds of channels and capture thousands of readings per second. These rates are on par with high-end benchtop multimeters and specialized instruments.

Powerful test synchronization

Tests that involve a large number of simultaneous measurements must precisely orchestrate external systems (like power supplies), DUTs, and instruments. Switch modules in data loggers allow entire sets of channels to be activated or deactivated. This is useful when different DUTs or subsystems must be activated in specific sequences.

To facilitate such synchronization, modern data loggers support increasingly sophisticated event detection, graphical test sequence diagramming, and instrument programming.

Dynamic data acquisition

Traditional data loggers only support static acquisition where they measure each channel just once per scan.

In contrast, modern data loggers support dynamicdata acquisition where each channel is measured multiple times per scan. This enables the detection of transient events in power and data signals. Dynamic phenomena like vibrations and noise can also be more accurately characterized.

Multiple domain measurements

Data loggers simultaneously support time-domain and frequency-domain analog measurements as well as digital-domain and physical measurements. This enables the all-around characterization of mixed-signal, RF, and electromechanical systems, which is essential for the final qualification and compliance testing stages.

What types of data can a data logger record?

Data loggers can measure a variety of parameters by combining their generic acquisition capabilities with suitable sensors.

Supported electrical measurements include the following:

Data loggers support these physical parameters:

How do you select the right data logger for a specific application?

Data Loggers:Keysight 34980A Daq | How Do You Select the Right Data Logger for a Specific Application?

Figure 3. Keysight 34980A DAQ

Some helpful tips for selecting a data logger are listed below:

How is data from a logger stored, retrieved, and analyzed?

Measured data are first stored with timestamps in the data logger's internal memory. For example, the DAQ970A and DAQ973A can store up to 1 million readings.

The measured data can be retrieved to a connected computer via ethernet, USB, or general-purpose interface bus (GPIB). Standard commands for programmable instruments (SCPI) like "FETCh?" are used to retrieve the data to the computer.

Alternatively, some loggers can store the readings on a universal serial bus (USB) flash drive for expanded capacity. The data can be downloaded as files.

Data loggers with displays and user controls support onboard channel configuration and analyses. Some data loggers support computed or virtual channels that calculate data from multiple channels in real time.

However, most engineers prefer using software like the PathWave BenchVueData Acquisition App from a connected computer for more complex setups and analyses.

Going forward, data loggers will be able to measure many more types of phenomena with increased scalability. Some key emerging trends are outlined below:

Deploy Keysight data loggers for your future needs

Keysight Daq Products | Deploy Keysight Data Loggers for Your Future Needs | Prcie vs Performance Image

Figure 4. Keysight DAQ products

In this blog post, you obtained an overview of data loggers, their applications, and their capabilities.

Keysight's DAQ systems anddata loggers cater to the special needs of critical industries like automotive, aerospace, defense, and health care.

Contact us for insights and help on data logger instruments and software.

limit
3