E23-em8a1
CVSS:
9.8 CVSS:3.1/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2022
Description
This strike exploits a code injection vulnerability in GLPI. The vulnerability is due to improper validation of user
configuration data sent to the endpoint htmLawedTest.php.
A remote unauthenticated attacker could exploit this vulnerability by sending a crafted request to the target server.
Successful exploitation could result in arbitrary code execution in the security context of the web server process.
*NOTE: While running this strike in OneArm mode, a file /tmp/poc is created on the server.
CVE
References
https://github.com/cosad3s/CVE-2022-35914-poc