Next-Generation Infiniium User Interface

Data Sheets

Keysight Technologies

Next-Generation Infiniium User Interface

Time for a Change

In 1997, Keysight Technologies, Inc. introduced its first Infiniium user interface.

Since then, Infiniium oscilloscopes have seen many innovations. It was the first line to release 33 and 63 GHz scopes and the only line to feature 1 and 2 Gpts oscilloscopes. It also released many award-winning applications like EZJIT, EZJIT Plus, SDA, InfiniiScan, InfiniiSim, PrecisionProbe, and Serial Data Equalization. Now it’s time for a user interface revolution to complement the Infiniium oscilloscopes’ history of innovation.

The new user interface delivers:

  •  Personalized viewing
  •  Better, faster documentation
  •  Best usability, including touch

Continuing the legacy of greatness

More than two years of research went into creating this user interface. One of the biggest pieces of advice that the Infiniium research team received was not to mess up what makes Infiniium real-time oscilloscopes great. Keysight oscilloscopes are intuitive to use, making it easier for users to quickly become scope experts. We didn’t want to lose this important feature, so the new user interface will use the same SCPI commands, easy-to-use wizards, and familiar menu system. But now measurements that used to take four screen shots and setups to make can be done with a single screen shot, saving you valuable time.

Display Data Like Never Before

The new user interface significantly improves your oscilloscope user experience. An FFT drives like a spectrum analyzer. You can manipulate function scales and time bases without having to use the function menu. Measurements are easier to view, and you can use many displays at any screen resolution that you want.

This user interface has more than 30 features that have never existed before on an oscilloscope. The user interface has an unmatched 128 grids, all with their own signal-to-noise ratio. (The previous industry high was 16 grids.) Every signal can be turned into its own real time eye.

Finally, everything that you do on the oscilloscope can be done on your PC!

Next-Generation Infiniium New User

1. Displayed vertical scale*

2. Measurement callouts*

3. Large icons for easy touch control*

4. Drag-and-drop measurements*

5. FFT bandwidth scale*

6. FFT peak callouts**

7. Tabbed window layout*

8. Timescale display*

9. Up to 16 grids per waveform are**

10. Up to 8 waveform areas*

11. Analysis charts for easy jitter analysis**

12. Undockable chart windows*

13. Tailfit vs. spectral char*

14. Memory display bar*

15. Dockable/floating measurement window*

16. Display up to 20 measurements**

17. Full statistic controls

18. Displayed marker measurements

19. Handles for touch control*

20. Color grade per signal**

21. Up to 16 real time eyes**

22. Slider bar*

23. Timescale per eye

24. Signal versus display control

25. Multiple right click controls

26. Windows multi-touch (gestures)*

27. Plus much more

Personalized Viewing

Slider bar and tabbed viewing

Windows flexibility has never been a part of a user interface before now. The Infiniium user interface is the first to allow windows to be resized by simply moving a slider bar. Take the flexibility one step further by choosing tabbed viewing and float your window. Each waveform area then has the ability to be floated to separate displays. Use this mode to increase your productivity by seeing waveform signals at the same time you use in-depth analysis charts.