*** *** PLEASE NOTE: There is a maintenance activity scheduled for 11th May 05:00 PM to 12th May 01:00 AM MST/12th Feb 4:30 AM to 12:30 PM IST. KC will be unavailable during this time window. *** ***

  

Main Support:       Knowledge Center
Documentation:   MBP English Doc   >  Previous Supported Releases   >  MBP 2016.01   >  MBP 2016_01 Release Notes

This document contains references to Agilent Technologies. Agilent's former Test and Measurement business has become Keysight Technologies. For more information, go to www.keysight.com.


MBP 2016.01 Release Notes

The MBP 2016.01 contains integrated data flow, BSIM-CMG and BSIM6 baseband model extraction flow, enhancements on Statistical modeling, and all defect fixes from the previous releases.

For general information about MBP, visit Keysight EEsof product web-page at:
http://www.keysight.com/find/eesof-products

Licensing

  • SHORT_PRODUCT_NAME requires: a) version 2015.05 of the EEsof EDA licensing software, b) version 3.2 codewords to run, and c) the licensing server software, lmgrd and agileesofd, to be upgraded to at least the same versions as what are included in EEsof EDA Licensing software 2015.05 SHORT_PRODUCT_NAME will not start if any of these requirements is not met. Refer to the License Codeword Version Compatibility Table.
  • In the EEsof EDA License Tools version 2015.05, licensing vendor daemon (agileesofd) is upgraded to sync up with FlexNet FNP 11.11.1.2 version of FLEX license manager (lmgrd).  SHORT_PRODUCT_NAME installer for the Windows platform will automatically set up these two new license server daemons by default for the local node-locked license users; for Linux, you need to follow the Linux/Solaris Licensing Setup instruction to complete the licensing configuration process. For more details, refer to Licensing (For Administrators).
  • A real-time and systematic license setup troubleshooting utility, Diagnose, is added to the License Manager tool. This utility produces a detailed health report of a user's currently configured licensing environment.
  • My Support ID utility is added to the License manager tool to allow a user to retrieve his/her Support ID required to contact Keysight EEsof Tech Support.

Enhancements and Improvements

  • For simplified and robust licensing, PJC (Per Job Control) licenses are no longer checked out by  SHORT_PRODUCT_NAME.
  • The License Setup Wizard no longer requires Administrator privilege on Windows to setup license files. Administrator privilege is only required to setup the windows service that will automatically start the license server upon system restart rather than on EEsof application startup.

Operating System Support

As previously announced, the Solaris (SUN OS) platform support has been discontinued and MBP 2013.01 is only supported on the LINUX Red Hat and Windows® operating systems.

Supported Windows and Linux platform

OS and Version

Windows XP

Windows 7 Enterprise

Windows 8 Enterprise

RedHat Linux RHEL4

RedHat Linux RHEL5

RedHat Linux RHEL6

Solaris 10 license Server

32/64 bit
32/64
32
64
32
64
64
64
64
64

MBP 2011.2.0

MBP 2012.07

MBP 2013.01

MBP 2014.04

MBP 2016.01
 

Legend

Description

Supported

Unsupported

New Features

  • Support 64bit system

  • New Feature of Corner tweaking system

    • Allow user to load corner models from a library, or generate a library from TT model as starting corner models.

    • User can view and edit corner spec table directly in MBP, and export to excel

    • Show the trend plot and polygon plot to tweak and do optimization

     

Other Enhancements and Improvements

  • Enhanced Mismatch plot function

    • Support Slope vs. W/L plot

    • Support customized mismatch plot X axis

  • Add warning message for clear page and clear pin function

Issues Fixed

  • Fix equation viewer defect when loading different temperature data with subckt model

  • Fix a SPECTRE simulation defect with internal engine

Licensing

  • On windows, a possible Administrator privilege issue preventing the automatic restarting of the FlexFNP license server program, lmgrd after the PC comes out of the hibernation mode has been fixed. The License Setup Wizard will automatically restart the server without any user intervention.
  • Unable to setup PathWave Model Builder (MBP) Licenses using License Setup Wizard 

  • Unable to setup MBP Licenses using License Setup Wizard

Known Issues - Licensing


  • You may observe additional License Usage when Client Machine reconnects to network after intermittent disruption.
    Workaround:  In case of network interruption on the client machine, to reclaim the inactive licenses, a TIMEOUT can be set using the TIMEOUTALL feature in options file (minimum time period of 15 minutes). The inactive license may stay checked out for this period of time

  • Unable to install Licensing Hardware Key Drivers on Windows.

  • Workarounds:

    • Turn off UEFI Secure Boot (BIOS) and use the default 6.3 version of the Wibu key driver delivered with the EEsof Licensing tools.

    • Turn on UEFI Secure Boot (BIOS), upgrade to ADS 2020 Update 2.0 and use the 6.51 WibuKey driver version available in the 2020.02 License tools installation directory.

    You will not be able to run older ADS releases with the 6.51 WibuKey dongle drivers

  • Setting FLEXLM_DIAGNOSTICS to the highest level (FLEXLM_DIAGNOSTICS=3) on Windows client may cause a crash during license checkout. Flexera is investigating this issue.
    Workaround:  It is recommended not to use the FLEXLM_DIAGNOSTICS on Windows clients or use it at lower level (FLEXLM_DIAGNOSTICS=1 or FLEXLM_DIAGNOSTICS=2).
  • Licensing may not support a license file path that is too long. This will likely occur when you have too many license files.
    Workaround:  Remove some license files, move the license files to a shorter directory path or to combine license files into a single file.

  • License Setup wizard may not be able to start license server with many license files. During setup, it may lead to a situation where a command prompt window appears/disappears incessantly. This is due to the fact that License Setup wizard is not able to start lmgrd with a long command line and may get stuck in a loop.
    Workaround: 

    1. It is recommended to combine all license code words tied to same MAC ID into single license file to avoid setting large number of license files.
    2. Try to use a shorter path to place license files.
    3. If  #1  and/or  #2  does not help, start the license server (lmgrd.exe) from the command line (e.g. lmgrd.exe -c <lic-file-path> -l <license_server_log.txt>) and then set <PRODUCT>_LICENSE_FILE=<PORT-NUMBER>@localhost for product you want to use on same PC.
  • Dongle drivers for Flex-10 dongles on Linux are release specific. Installing the latest dongle drivers on Linux will function properly only for the most recent EEsof releases.
    Workaround
    : Install and use dongle drivers as needed.  If you need to run the most recent EEsof releases, use the latest  Flex-10 dongle driver. If you need to use older releases, uninstall the latest dongle driver and re-install the older dongle driver

  • FLO and EEsof License setup are writing server logs at different locations. However, the EEsof server log file location is updated in the License Manager > Environment tab.
  • When multiple  same-named  INCREMENT lines  of different version  exist on the license server, few advanced FlexNet options to reserve/limit licenses may not work properly. 
  • Product Selector “Check Availability“ generates incorrect results (which leads to license failure) for older releases when multiple date base versions of like-named bundles exist in the license pool.
  • In Linux, Product Selector  OK  and  Cancel  Buttons locations are reserved.
  • Starting from FlexNet Publisher 2015 (also known as version 11.13.1), the adoption of the best practice of the least-privilege security therein results in the License Server related Windows Service to run with the LocalService Account privilege (instead of the LocalSystem privilege as before.)  Running with the LocalService Account privilege, an executable can no longer access any files located in the per-user specific type of folders.  As a result, any license file placed in those folders can no longer be accessed by the License Server when the License Server is automatically started via the Windows Service upon each PC reboot. For the local node-locked license, this would not result in any disruption to the usage of EEsof applications; however, for the license installed on a network PC that is accessed by multiple client PCs, this may cause EEsof applications not to start after the network PC reboots
    Workaround: Store your license files in the Windows folders that are accessible by the LocalService Account privilege.  For example, C:\ProgramData or C:\users\public are both qualified choices.  In general, any folder that has the "Users" group listed in its Properties > Security page and this "Users" group has the  read  permission enabled should work. 
  • Using the default port to connect to a license server may cause a delay when checking out licenses. If no port is given in the license file, Flexera scans ports 27000 to 27009 to find the port. Starting from FlexNet Publisher 2015 (aka version 11.13.1), the default timeout for the response from each port increased from .1 seconds to 3 seconds.

    To avoid the delay, KSM now issues licenses with port 27009 instead of leaving this blank. The EEsof License Setup Wizard (from Licensing 2017.01 onwards) handles some common situations such as: where it detects license file(s) without port, when users get a new license file with port 27009, or when all license files for a vendor daemon does not have same port.

    You will not be able to start the license server if all license files for a vendor daemon on a server does not have same port.
    Users who manually setup a license server or using EEsof License Setup Wizard with older licensing bits may need to manually edit license files to comply with the following rules:

    1. All license files for a vendor daemon on a server must use the same port (or all be blank). 

    2. Using the default port (blank) is allowed but may result in longer checkout times. 

    3. If setting up a network server, select an unused port that is not blocked by a firewall.

    Workaround:  If the user cannot change the port, or wants to use the default Flexera ports, the environment variable FLEXLM_TIMEOUT can be set to .2 seconds (200000), to minimize the performance degradation. However, if the network latency is an issue in your environment, you may need to fine-tune this setting to minimize the general performance degradation while still accommodating the network latency.

  • Installation of EESof EDA tools (such as, SystemVue 2016.08, Genesys 2017.XX, or ADS 2017.XX) may hang at 4% (percentage vary based on the products) for few hours or even more on some specific machines.
    Workarounds:
    • Disable Firewall setting in Anti-Virus Software installed on the PC.
      or
    • Download and unzip process explorer from the below link and then invoke  procexp.exe.
      https://docs.microsoft.com/en-us/sysinternals/downloads/process-explorer
      Right click on the  wusa.exe  process under <Product installer exe> and select KillProcess. Now it will continue the product installation.
  • After installing EESof EDA tools (such as, SystemVue 2016.08, Genesys 2017.XX, or ADS 2017.XX) successfully and try to invoke the software or License wizard, you may encounter “api-ms-win-crt-runtime-l1-1-0.dll” missing error.

    Workaround:  Install the Update for Universal C Runtime in Windows .  On Windows 64-bit system systems, the file to install is x64 version of the Microsoft hotfix KB2999226. A copy of the Windows6.1-KB2999226-x64.msu Microsoft 64-bit hotfix installer can be found under the  C:\Program Files\Keysight\EEsof_License_Tools\bin  directory.  The Microsoft hotfix KB2999226 can be found under the Update for Universal C Runtime in Windows  page at  https://support.microsoft.com/en-us/help/2999226/update-for-universal-c-runtime-in-windows as well.
  • On a newly formatted RHEL system, the EEsof Licensing tools may fail to boot. This is because the FlexNet Publisher 2015 requires a certain rpm
    Workaround:  Under the EEsof product installation directory, there exists a utility script named "Linux_sys_check.sh"  under the  bin  directory. Run this script to find out whether any rpm is missing; run this script with a "-y" command-line option to also have all the missing rpms automatically installed if you have the  sudo  or  root  privilege.
  • License server may stop recognizing Flex-10 dongle on some systems within a few hours after starting
    Workaround: If v6.10 or v6.11 is found and experience this problem then upgrade the WibuKey drivers to v6.30/6.30b from Wibu Systems.
  • Unable to install Flex-10 driver if Flex-9 dongle is already plugged into a machine
    Workaround: Before installing a Flex-10 driver for the first time, unplug the Flex-9 dongle.
  • There is a known FlexNet Publisher issue, whereby mixing node-locked codewords and floating codewords in one license file can result in: a) Remote simulations not working or b) A second local simulation not working in case the license is node-locked and also has incorrect version.
    Workaround: It is strongly recommended that you do not mix node-locked codewords and floating codewords in one license file nor in  any  configuration that ends up with node-locked codewords and floating codewords both available on the same server. In other words, put the node-locked license and the floating license on different servers, and point to the respective one based on what you need to run.
  • If a user simultaneously runs two instances of a product and has mixed different versions of the same codeword on one license server, extra licenses may be pulled and result in unexpected “Licensed number of users already reached for this feature” errors.
    Workaround: We recommend you remove expired codewords, to separate out the new and the old versions of codewords into different files and different servers, and to point to the respective one based on what you need to run.
  • Not specifying the TCP/IP port for the license server during license setup may lead to unexpected behavior and/or license checkout failure on the Windows platform. We strongly recommend you to always explicitly specify the TCP/IP port associated with each license server.
  • A node-locked and floating bundle operating on Linux cannot be shared between products using EDA License Tools version older than 2014.01 when run at the same time.
  • License Setup Wizard does not remove any previous user-configured FLEX Windows License Service manually set up by a user using FlexNet's lmtools.
    Workaround: You must remove the previous user-configured Windows License Service via lmtools.
    • Run the lmtools.exe from  C:\Program Files\Agilent\EEsof_License_Tools\bin  to invoke the lmtools utility. The lmtools utility window is displayed.

      If you have installed an EEsof product released before 1st  August, 2014 on your system prior to installing an EEsof product released after 1st  August, 2014 then the default EEsof Licensing tools path will remain  C:\Program Files\Agilent\EEsof_License_Tools.  On the systems that only have EEsof products released after 1st  August, 2014 installed then the default EEsof Licensing tools path will be  C:\Program Files\Keysight\EEsof_License_Tools.
    • In the  Service/License File  tab, check the  Configuration using Services  option. All user-configured FLEX Windows License Services will be listed.
    • Select the service you wish to remove.
    • Select the  Config Services  tab and click the  Remove Service  button to remove the service.
      To ensure that the license service or  lmgrd   is running, click  View Log. A log window appears that confirms whether  agileesofd   and  lmgrd   are up and running.
  • While running multiple versions of prior  SHORT_PRODUCT_NAME  releases together, set  PRODUCT_NAME_MAXIMUM_BUNDLE_USAGE=ON in your environment so that all of them will use the same method to check out licenses. Otherwise, you might receive an error message, "Licensed number of users already reached".
  • For LSF style distributed simulations, ensure that the PATH on the client computer points to the $HPEESOF_DIR/EEsof_License_Tools/${architecture} directory that corresponds to the EEsof release being used. This needs to be done in order to ensure that the proper version of the Flexera utilities (like  lmutil) gets picked up in the path before any older in-compatible versions (that may also be installed on a users’ system.)
  • License Setup Wizard (aglmwizard.exe), which is used to set up and record the license path would not work if you already have an environment variable set for  PRODUCT_NAME_LICENSE_FILE.
    Workaround:  You can use PRODUCT_NAME_LICENSE_FILE variable to point to license file or refer to Licensing (For Administrators).
  • The License Setup Wizard will exit or not properly configure a license server, if the server has all of its licenses currently in use.
    Workaround:  Wait for a license on the server to become available as you normally would before launching the product.
  • Unable to set license in case unicode characters are used either in path or license file name because the Flex License Service does not support these characters.
  • The Product Selector tool will be unable to display the license server status properly when connected to older license server.
    Workaround: Upgrade your license server to the latest version.

  • EEsof Licensing Tools installer can hang on systems with McAfee LiveSafe installed and running the default firewall settings.
    Workaround:   Prior to installing EEsof Licensing Tools, temporarily turn off the McAfee LiveSafe firewall.

  • Licensing setup steps on systems with McAfee LiveSafe installed can fail.
    Workaround:  Under the McAfee LiveSafe firewall settings, under Port and Settings, allow the use of port 27001 for lmgrd.exe under the EEsof Licensing Tools installation bin directory.  Under Internet Connections for Programs , enable lmgrd.exe, aglmmgr.exe and aglmwizard.exe for all devices and turn off monitoring.

  • On Windows, EEsof product releases prior to 2014 can have boot time issues with licensing if an newer EEsof product is installed prior to installing the older product. For example, if a users installs Advanced Design System 2017 and then installs Advanced Design systems 2014.01, the user can have boot time errors with ADS 2014.01.
    Workaround:  For Advanced Design System users,  set a system environmental variable named ADS_LICENSE_FILE under the Control Panel/ System, and Security / System / Advanced system settings and under the "environmental variables".  Add an System variable named ADS_LICENESE_FILE and the value will be the path to your local license file or the port@host setting for your site.


Please help us improve
Please help us improve
Was this topic helpful?