Technical Overviews
This certifies that the equipment has been calibrated using applicable Keysight Technologies procedures and accredited to ISO/IEC 17025:2005. The quality management system is registered to ISO 9001:2008.
As Received Conditions
The expanded measurement uncertainty intervals about one or more measured values were in as well as out of specification. Consequently, neither compliance nor non-compliance with specification can be declared based on the stated coverage probability.
Action Taken
- The equipment was adjusted.
As Completed Conditions
The measured values of the equipment were observed in specification at the points tested. Additionally, the expanded measurement uncertainty intervals about the measured values were in specification.
Remarks or Special Requirements
This calibration certificate may refer to instruments manufactured by HP, Agilent and Keysight as being manufactured by Keysight Technologies, Inc. The test limits stated in the report correspond to the published specifications of the equipment, at the points tested
Compliance with Specification
The uncertainty of measurement has been taken into account when determining compliance with specification, as per ILAC-G8:03/2009. If the expanded measurement uncertainty intervals centered about one or more measured values were both in as well as out of specification (upper or lower), it is not possible to state compliance or non-compliance based on a 95% coverage probability for the expanded measurement uncertainty. An overall statement of compliance for all tests performed as received, and as completed (if any adjustments / repairs were performed) is included at the beginning of this report. Statements of compliance apply only to warranted specifications. When functional verification tests are performed, results are reported in the “Functional Test” section, and do not affect these statements of compliance. The status summaries relate to the tested item only. A final decision about whether the item's performance actually satisfies requirements of the user can only be made by the user.
Measurement results are reported as:
• Passed ( ) - The measured values of the equipment were observed in specification at the points tested. Additionally, the expanded measurement uncertainty intervals about the measured values were in specification.
• Undetermined (U) - The expanded measurement uncertainty intervals about one or more measured values were in as well as out of specification. Consequently, neither compliance nor non-compliance with specification can be declared based on the stated coverage probability.
• Failed (F) - One or more measured values of the equipment were observed out of specification at the points tested. Additionally, the expanded measurement uncertainty intervals about one or more measured values were entirely outside the specification.
Acceptance Limit
The "Keysight Cal + Uncertainties + Guardbanding" service employs a guard band in the amount of the 95% expanded measurement uncertainty (MU). The resulting acceptance limit applied for Pass or Fail decisions, and for performing adjustments, is the difference of the specification and the guard band.
Uncertainty of Measurement
The uncertainty evaluation has been performed in accordance with ISO/IEC Guide 98-3:2008 (GUM). The reported expanded measurement uncertainty, which corresponds to a coverage probability of approximately 95%, is the standard uncertainty multiplied by the coverage factor k=2. Where this is not the case, coverage factor (k), effective degrees of freedom (veff) and coverage probability (p) are stated.
×
Please have a salesperson contact me.
*Indicates required field
Thank you
A sales representative will contact you soon.
What are you looking for?