Official Used
Equipment Store

Keysight Oscilloscope Glossary

What Is Ohm’s Law?

How do you know how much current will flow through a circuit when you apply a voltage? Or how adding resistance affects electrical performance? 

These aren’t just theoretical questions, they are essential for designing, troubleshooting, and optimizing electrical systems. The answer lies in Ohm’s Law, one of the most fundamental principles in electrical engineering. 

Whether you are working with power distribution, circuit design, or testing equipment, understanding Ohm’s Law allows you to predict and control electrical behavior with precision.

Key Takeaway
Ohm’s Law defines the relationship between voltage, current, and resistance, making it essential for circuit analysis, design, and troubleshooting. Understanding and applying this principle allows you to predict electrical behavior and ensure optimal system performance.

Understanding Ohm's Law

Ohm's Law defines the linear relationship between voltage (V), current (I), and resistance (R) in an electrical circuit. 

Formulated by German physicist Georg Simon Ohm in 1827, the law states that the current flowing through a conductor is directly proportional to the voltage across it and inversely proportional to its resistance. Mathematically, you can express this relationship as:

V = I × R

Where:

  • V is the voltage in volts (V),
  • I is the current in amperes (A),
  • R is the resistance in ohms (Ω).

This equation implies that if you increase the voltage across a conductor, the current will increase proportionally, provided the resistance remains constant. Conversely, increasing the resistance will result in a decrease in current for a given voltage.

MSOX Oscilloscopes

Precision You Can Trust

See MSOX 3000 Series Offers

Practical Applications of Ohm's Law

Ohm’s Law is not just a theoretical equation—it’s a tool you use daily in electrical engineering and circuit design. 

Whether you're designing a new circuit, diagnosing a malfunction, or selecting components, this fundamental principle helps you make informed decisions.

1. Circuit Analysis

Understanding how voltage, current, and resistance interact allows you to analyze both simple and complex circuits efficiently. You can:

  • Determine missing values: If you know two of the three parameters (voltage, current, or resistance), you can calculate the third.
  • Verify circuit functionality: Checking measured values against expected calculations helps confirm if a circuit is working correctly.
  • Predict power consumption: Using the power equation P = V × I, you can calculate how much power a device will consume or generate.

2. Component Specification

Selecting the right components for a circuit ensures performance, longevity, and safety. Ohm’s Law helps you:

  • Choose appropriate resistor values: If you need to drop voltage to protect sensitive components, you can calculate the correct resistance.
  • Select power ratings: Knowing the current and voltage in a circuit allows you to choose components that can handle the required power dissipation.
  • Prevent overheating and failures: Overloading a resistor or capacitor with excess voltage or current can cause damage; Ohm’s Law helps you prevent this by ensuring proper ratings.

3. Troubleshooting and Fault Detection

Ohm’s Law is crucial for diagnosing issues in electrical circuits. When a system is malfunctioning, measuring voltage and current can reveal:

  • Short circuits: If current is unexpectedly high, a short circuit may be present, causing resistance to drop abnormally.
  • Open circuits: If no current flows despite applied voltage, a break or faulty connection in the circuit is likely.
  • Component degradation: Over time, resistors and other components can drift from their rated values, affecting performance. Checking resistance can help identify failing components.

4. Power Distribution and Load Management

In power distribution, engineers use Ohm’s Law to ensure circuits operate efficiently without overloading power sources. By calculating current draw, you can:

  • Design power grids that balance load across multiple circuits
  • Determine wire gauge sizes to handle specific current levels without excessive voltage drop
  • Optimize energy efficiency in industrial and consumer electronics
     

5. Testing and Measurement

Using oscilloscopes, multimeters, and other test equipment, you can verify Ohm’s Law in real-world applications. Whether you're testing PCBs, power supplies, or embedded systems, measuring voltage and current lets you:

  • Confirm expected resistance values
  • Monitor fluctuations in electrical behavior under different loads
  • Validate theoretical calculations with real-world performance data

By applying Ohm’s Law across these various areas, you can build more reliable circuits, solve electrical problems faster, and ensure safety in your designs.

Ohm's Law in Series and Parallel Circuits

Understanding how Ohm's Law applies to different circuit configurations is crucial.

Series Circuits

In a series circuit, components are connected end-to-end, so the same current flows through each component. The total resistance (Rtotal) is the sum of individual resistances:

Rtotal = R₁ + R₂ + R₃ + ... + Rₙ

The voltage drop across each component can be calculated using Ohm's Law, and the sum of these voltage drops equals the total applied voltage.

Parallel Circuits

In a parallel circuit, components are connected across the same two points, providing multiple paths for current. The total resistance can be found using:

1/Rtotal = 1/R₁ + 1/R₂ + 1/R₃ + ... + 1/Rₙ

In this configuration, the voltage across each component is the same, but the currents through each path can differ.

Equipment for Verifying Ohm’s Law

To measure voltage, current, and resistance accurately, use the following instruments:

  • Digital Multimeter (DMM): Measures voltage, current, and resistance directly, making it the simplest and most precise tool for verifying Ohm’s Law.
  • Ammeter: Measures current directly in a circuit, particularly useful for DC applications.
  • Power Analyzer: Measures voltage, current, resistance, and power consumption, ideal for both AC and DC circuits.
  • Oscilloscope with a Current Probe: Useful for observing real-time voltage and current waveforms, particularly in AC circuits or when analyzing transient signals.
  • Shunt Resistor with an Oscilloscope: Allows current measurement by placing a precision low-value resistor in series with the circuit and measuring the voltage drop across it.

Testing Process

  1. Set up the circuit
    • Connect a known resistor to a variable DC power supply.
    • Use precision resistors with a low tolerance (1% or better) to ensure accurate readings.
  2. Measure voltage
    • Use a DMM to measure the voltage across the resistor.
    • If using an oscilloscope, probe both ends of the resistor to observe the voltage waveform.
  3. Measure current
    • Place a DMM or an ammeter in series with the circuit to measure current directly.
    • If using an oscilloscope, add a shunt resistor in series and measure the voltage drop across it, then calculate current using I = Vshunt / Rshunt.
    • Alternatively, use a current probe with an oscilloscope for real-time current waveform analysis.
  4. Adjust and observe
    • Vary the input voltage and record the corresponding current values.
    • Plot voltage versus current. If the relationship follows Ohm’s Law, the graph will be a straight line with a slope equal to the resistance value (R = V / I).

Limitations of Ohm’s Law

While Ohm’s Law is fundamental to electrical engineering, it does not apply universally. Several factors can affect its accuracy in real-world applications.

Non-Ohmic Materials

Devices like diodes, transistors, and vacuum tubes do not exhibit a linear voltage-current (V-I) relationship. Unlike resistors, whose resistance remains constant, these components have variable resistance depending on voltage, current, or external influences, meaning Ohm’s Law cannot be directly applied. Instead, more complex models, such as diode equations or transistor operating regions, must be used.
 

Temperature Variations

Resistance in many materials changes with temperature. For example, metals generally have a positive temperature coefficient, meaning resistance increases as temperature rises. 

In contrast, semiconductors and thermistors can exhibit a negative temperature coefficient, where resistance decreases with rising temperature. This variability means that Ohm’s Law may not hold precisely in circuits where temperature fluctuations are significant.

High-Frequency AC Circuits

In circuits with alternating current (AC), resistance is not the only factor affecting current flow. Inductors and capacitors introduce reactance, which, together with resistance, forms impedance (Z). 

In such cases, Ohm’s Law must be extended to its AC form: V = I × Z, where Z accounts for both resistance and reactance. At high frequencies, phase shifts between voltage and current must also be considered, requiring complex impedance analysis.

Key Relationships in Ohm's Law

Quantity

Symbol

Formula

Unit

Voltage

V

V = I × R

Volts (V)

Current

I

I = V / R

Amperes (A)

Resistance

R

R = V / I

Ohms (Ω)

Power

P

P = V × I

Watts (W)

 

Oscilloscopes

Solve Signal Issues Before They Escalate

See MXR608A Special Offers

Conclusion

Ohm’s Law is essential for analyzing, designing, and troubleshooting electrical circuits. Understanding the relationship between voltage, current, and resistance allows you to select the right components, detect faults, and optimize system performance. 

Whether you’re verifying circuit behavior or ensuring accurate power distribution, reliable measurement tools make a difference.

Accurate testing requires reliable measurement tools. If you need high-quality oscilloscopes, spectrum analyzers, function generators, or multimeters, check out Keysight’s Premium Used Equipment Store for certified pre-owned instruments that deliver precision at a lower cost.

Whenever You’re Ready, Here Are 5 Ways We Can Help You

  1. Browse our Premium Used Oscilloscopes.
  2. Call tech support US: +1 800 829-4444 
    Press #, then 2. Hours: 7 am – 5 pm MT, Mon– Fri
  3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
  4. Create an account to get price alerts and access to exclusive waitlists.
  5. Talk to your account manager about your specific needs.

Subscribe to Get Our Latest News, Updates, and Articles.

Get Email Updates