Official Used
Equipment Store

Keysight Oscilloscope Glossary

What Is Directivity?

Have you ever wondered why some antennas seem to focus their energy in one direction while others spread it out equally in all directions? The answer lies in directivity, a crucial concept in signal transmission and reception. 
Whether you are working with antennas, spectrum analyzers or network analyzers, understanding directivity can greatly improve your ability to fine-tune your systems for better performance.

Directivity Definition

Directivity is a measure of how well an antenna or device focuses energy in a particular direction compared to a reference, typically an isotropic radiator, which spreads energy equally in all directions. 
When an antenna has high directivity, it concentrates energy in a narrow beam, making it ideal for long-distance communications or focused signal transmission. 
Low-directivity antennas, on the other hand, radiate more uniformly, which may be beneficial for applications requiring broader coverage.

Key Takeaway
Directivity measures how effectively an antenna or device focuses energy in a specific direction, improving signal strength and reducing interference. High directivity is essential for applications requiring precise signal targeting and optimal performance in communication and testing systems

Key Concepts Behind Directivity

Directivity plays a key role in fields like antenna design, radiofrequency (RF) engineering, and signal measurement. Here are a few fundamental concepts to keep in mind:

  • Power radiation: Directivity is based on how much power is radiated in a specific direction relative to the total power output of the antenna.
  • Beamwidth: Beamwidth refers to the angular separation where the signal strength drops to half its peak value. Narrow beamwidth typically indicates higher directivity.
  • Gain: Gain combines directivity with the antenna’s efficiency in converting input power into radiated energy. An antenna may have high directivity but low gain if it suffers from losses.

The Importance of Directivity in Engineering

Directivity is crucial for several reasons:

  1. Improved signal strength: High-directivity devices focus energy on a target area, improving signal reception and transmission over longer distances.
  2. Interference reduction: By concentrating energy in a specific direction, high-directivity devices help minimize interference from unwanted signals.
  3. Efficiency in testing: Directivity plays a major role in RF testing and measurement, as it allows for more precise targeting and analysis of signals.

How to Measure Directivity

Measuring directivity involves determining how much power an antenna radiates in its main direction compared to all other directions. 
This measurement is essential for understanding how focused or spread out the radiated energy is. Directivity is usually expressed in decibels (dB), providing a logarithmic scale to easily compare values. The higher the directivity, the more concentrated the energy is in one direction.
To calculate directivity, engineers use the following formula:

Directivity: D = 4π / (Total Radiation Pattern)

Where:

  • D is the directivity (unitless).
  • 4π represents the total solid angle in all directions (in steradians).
  • Total Radiation Pattern refers to the integration of the antenna's power radiation over all angles (measured in steradians).

Once you have the directivity, you can convert it into decibels (dB) for easier comparison. To do this, use the following formula:

Directivity in dB:

D(dB) = 10log10(D)

Steps to Measure Directivity:

  1. Measure radiated power in the main direction: Use appropriate testing equipment, such as a signal generator and an antenna, to measure the power output in the primary radiation direction (the direction of maximum gain).
  2. Determine total radiated power: Measure the total radiated power across all directions. This step typically involves rotating the antenna or using a measurement setup that captures signals in all directions.
  3. Calculate the directivity: Using the values obtained from the above steps, apply them to the formula D=4π/(TotalRadiationPattern) to find the directivity. This value gives you an idea of how much more power is radiated in the main direction compared to other directions.
  4. Convert to decibels: To make comparisons easier between different antennas or systems, convert the directivity to decibels using the formula D(dB)=10 x log10(D)

Why Measuring Directivity Matters

  • Precision in communication systems: High directivity allows systems to target signals precisely, minimizing wasted energy and increasing efficiency.
  • Optimized testing: In signal testing, directivity helps isolate specific signals, reducing interference and improving accuracy.

Accurate directivity measurements ensure that your systems are functioning optimally, whether you're designing communication systems, testing RF signals, or working on antennas for specialized applications.

Directivity vs. Gain: What's the Difference?

While directivity measures how well energy is focused in a particular direction, gain takes into account the efficiency of the antenna in converting power into radiation. The main difference is that directivity refers only to the pattern of energy distribution, while gain includes both directivity and losses within the system.

AspectDirectivityGain
DefinitionFocus of energy in one directionEfficiency in radiating power
MeasurementPurely geometric or spatialTakes into account system losses
ImportanceDetermines signal targetingAffects overall system efficiency

Practical Applications of Directivity

Directivity has wide-ranging applications, from designing communication systems to optimizing RF testing. Here are some common scenarios where directivity comes into play:

  • Antenna design: Engineers use directivity to control how much energy is radiated in specific directions, especially in radar, satellite, and communication antennas.
  • RF testing: High-directivity devices are used in testing equipment to isolate signals and reduce interference when measuring system performance.
  • Microwave systems: Directivity in microwave antennas ensures that the transmitted power reaches the target with minimal loss.

Types of Antennas Based on Directivity

Different types of antennas provide varying levels of directivity. Here’s a breakdown:

  1. Omnidirectional antennas: These antennas radiate energy equally in all directions. They are ideal for applications requiring broad coverage, such as Wi-Fi and broadcast systems.
  2. Directional antennas: These have higher directivity and are used for focused transmission. Examples include parabolic dishes and Yagi antennas, commonly used in satellite communications and television transmission.
  3. Patch antennas: These antennas provide moderate directivity and are often used in compact systems like mobile phones and GPS units.

Key Factors Affecting Directivity

Several factors can influence an antenna's directivity:

  • Size of the antenna: Larger antennas generally offer higher directivity, as they can focus energy more effectively.
  • Frequency of operation: Higher frequencies typically result in narrower beamwidths, leading to greater directivity.
  • Antenna shape and design: The physical design of the antenna, including the reflector and elements, plays a significant role in determining its directivity.

How Directivity Impacts Testing Equipment

Directivity plays a significant role in improving the performance and accuracy of various testing equipment. 
In testing environments, where precision is critical, high directivity enables engineers to focus on specific signal paths, reduce noise, and isolate the signal of interest. 
Let’s explore in more detail how directivity affects different types of testing equipment:

Spectrum Analyzers

A spectrum analyzer measures the amplitude of signals over a range of frequencies, making it essential for frequency analysis and identification. 
Directivity plays a key role here by helping the spectrum analyzer focus on the intended frequency range and reducing the potential for cross-interference from other signals or sources.

  • Frequency isolation: High-directivity antennas used in conjunction with spectrum analyzers can better isolate specific frequencies, allowing engineers to target particular bands without interference from adjacent frequencies.
  • Improved sensitivity: Directivity enhances the sensitivity of the spectrum analyzer by concentrating the reception on the desired signal, which is especially useful when dealing with weak or distant signals. This leads to more accurate readings of signal strength and frequency components.

Network Analyzers

Network analyzers are used to measure the response of circuits, components, and systems in terms of reflection and transmission properties. Directivity is crucial for network analyzers because it improves the accuracy of these measurements.

  • Reflection measurements: Directivity helps in reducing the impact of signal reflections that can distort measurements. High directivity minimizes reflections, making it easier to isolate the desired signal and obtain accurate S-parameter measurements.
  • Transmission accuracy: With high directivity, network analyzers can better measure how a signal transmits through a device under test, providing clearer insights into its performance characteristics.

Impact on Testing Efficiency

Directivity enhances measurement accuracy and significantly improves the overall efficiency of testing processes. By concentrating the measurement or transmission on the intended target, directivity allows engineers to:

  • Reduce setup time: Engineers spend less time adjusting testing equipment to avoid interference or unwanted signals. High directivity naturally filters out background noise, streamlining the testing process.
  • Increase reliability: More focused measurements lead to higher reliability in results, reducing the need for repeated testing due to errors caused by signal interference.
  • Minimize environmental interference: In complex testing environments, such as labs with multiple devices, directivity ensures that measurements are not contaminated by external signals or reflections from other equipment.

Conclusion

Directivity is a key concept that affects everything from antenna design to signal testing. Understanding how energy is focused and how to measure directivity can help you improve signal strength, reduce interference, and optimize your systems for better performance. 
Whether you're working with communication systems, RF testing, or designing antennas, directivity is a factor you can't ignore.
If you're looking to improve your testing capabilities, visit Keysight's Used Equipment Store. You'll find premium, pre-calibrated  oscilloscopes, spectrum analyzers, network analyzers, function generators, and multimeters—all at competitive prices. 

Get the accuracy and performance you need without the wait or high cost of new equipment.

Whenever You’re Ready, Here Are 5 Ways We Can Help You

  1. Browse our Premium Used Oscilloscopes.
  2. Call tech support US: +1 800 829-4444 
    Press #, then 2. Hours: 7 am – 5 pm MT, Mon– Fri
  3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
  4. Create an account to get price alerts and access to exclusive waitlists.
  5. Talk to your account manager about your specific needs.

Subscribe to Get Our Latest News, Updates, and Articles.

Get Email Updates