Keysight Oscilloscope Glossary
What Is a Time Interval in Oscilloscopes?
Introduction
Did you know that modern oscilloscopes can measure time intervals as small as a few nanoseconds or even picoseconds?
With the advent of faster and more complex electronics, it has become increasingly essential to understand time intervals and how oscilloscopes measure them.
Let's dive in to master the nuances of time intervals in oscilloscopes.
What Is a Time Interval?
A time interval, in the context of oscilloscopes, is the time difference between two specific events captured during waveform analysis. These events could be voltage transitions, current changes, or any other signal characteristic that you are observing.
Understanding and measuring time intervals accurately are crucial for:
- Debugging circuit timing issues
- Verifying signal integrity
- Optimizing the performance of your systems
Key Takeaway
Accurate time interval measurements hinge on understanding and optimizing key parameters like resolution, accuracy, and jitter, while also avoiding common pitfalls and following best practices.
Types of Time Intervals
Understanding the intricacies of different time intervals is essential for the precise characterization and troubleshooting of electrical and electronic systems.
There are fundamentally two categories to consider: Single Shot and Repetitive.
Each of these has distinct applications that require specific methodologies for accurate measurement.
Single Shot
Single-shot time intervals are indispensable in scenarios where the signal or event under consideration occurs only once or very sporadically.
This uniqueness or rarity of the event makes capturing and analyzing it challenging but also crucial.
Here's how single-shot time intervals typically come into play.
- Fault finding: When troubleshooting circuit anomalies or failures, single-shot time intervals can help identify the exact moment of a malfunction, aiding in the diagnostic process.
- Transient recording: Sudden changes in system state, such as startup or shutdown sequences, often require single-shot measurements. These intervals allow engineers to study these transient behaviors in detail.
- Non-repetitive signal analysis: For systems with irregular signals, such as certain types of communication signals or biological signals like ECGs, single-shot time intervals are essential for detailed analysis.
Repetitive
Repetitive time intervals are all about capturing periodic or recurring events. Given their cyclical nature, these types of intervals are common in systems that function based on clocked operations or synchronized activities.
Below are some common applications.
- Frequency measurement: One of the most straightforward applications for repetitive time intervals is determining the frequency of a periodic signal. By capturing multiple cycles and averaging the time between peaks, you can calculate the frequency with high accuracy.
- Phase difference calculations: In systems with multiple related signals, the phase difference between them is often a critical parameter. Repetitive time intervals help in measuring this difference to ensure proper synchronization.
- Cycle-to-cycle jitter evaluation: In digital and high-frequency systems, the consistency between cycles is crucial. Repetitive time intervals allow for the capture and analysis of these small deviations, known as jitter, which can have substantial implications on system performance and reliability.
The type of time interval—be it single-shot or repetitive—depends heavily on the specific needs of your application. Understanding the nuances of each can greatly enhance your ability to make precise measurements, thereby improving your system's performance and reliability.

Key Parameters and How to Measure Them
A precise and accurate measurement of time intervals in oscilloscopes revolves around a set of key parameters.
Each of these parameters not only influences the quality of the measurement but also the conclusions you can draw from the data.
Let's delve deeper into these critical factors: Resolution, Accuracy, and Jitter.
Resolution
Resolution refers to the smallest time increment that your oscilloscope can measure. The better the resolution, the more finely you can dissect your signals to understand rapid or subtle changes.
- How to measure: Typically, you can find the resolution in the oscilloscope’s specifications, often denoted in units like nanoseconds (ns) or picoseconds (ps).
- Considerations: High-resolution oscilloscopes usually come at a higher cost. Consider the needs of your application; sometimes, moderate resolution is adequate.
Accuracy
Accuracy is the degree to which the measured time interval aligns with the "true" or "actual" time interval of the event. A lack of accuracy can lead to misleading data and faulty conclusions.
- How to measure: Regularly calibrate your oscilloscope and compare your measurements with known standards to ascertain accuracy.
- Considerations: The calibration process should be consistent and should ideally use standards traceable to national or international references.
Jitter
Jitter involves the fluctuations or variations in time interval measurements when you measure the same signal multiple times. High jitter could be a sign of signal instability or noise interference.
- How to measure: Use the statistical functions available in modern oscilloscopes to analyze jitter. This usually provides metrics like mean value, standard deviation, and histograms.
- Considerations: If jitter is significant, consider improving your setup's grounding and shielding. Also, using averaging methods can help minimize jitter.
Measuring Techniques
There are various techniques you can employ to measure these parameters effectively:
- Direct reading: Activate the cursors on your oscilloscope's display to manually indicate the points between which you want to measure the time interval. The oscilloscope then calculates and displays the interval.
- Automated measurement: Modern oscilloscopes often come equipped with built-in functions that can automatically calculate time intervals, saving time and minimizing human error.
- Mathematical functions: For more complex analysis, you can apply mathematical transformations like Fast Fourier Transform (FFT) to your signal. This is particularly useful for identifying periodic components or filtering noise.
Method of Measurement for Each Parameter
| Parameter | Method of Measurement |
|---|---|
| Resolution | Consult the oscilloscope specifications |
| Accuracy | Perform calibration and compare with known standards |
| Jitter | Conduct a statistical analysis of multiple measurements |
Consult the oscilloscope specifications
Perform calibration and compare with known standards
Conduct a statistical analysis of multiple measurements
Understanding and effectively measuring these key parameters—resolution, accuracy, and jitter—can substantially improve your time interval analyses.
Tailoring your measurement techniques to the specific needs of your application can further optimize your data collection process, providing you with the most accurate and insightful results.
Common Misakes to Avoid
The seemingly simple task of measuring time intervals with an oscilloscope can be fraught with pitfalls if you're not careful. Attention to detail is crucial, as small errors can lead to significant inaccuracies.
Here are some common mistakes to avoid and how you can sidestep them:
Insufficient Bandwidth
The bandwidth of an oscilloscope determines the range of frequencies it can accurately measure. If the bandwidth is too low for your target signals, you'll end up with distorted or incomplete information.
- How to avoid: Always check the oscilloscope's bandwidth against the frequency components of your signal. A general rule of thumb is to choose an oscilloscope with a bandwidth at least five times higher than the frequency of the signal you are measuring.
- Implications: Using an oscilloscope with insufficient bandwidth can cause you to miss high-frequency components, leading to incomplete or incorrect analysis. This is particularly concerning in high-speed digital circuits and RF applications.
Incorrect Triggering
Triggering stabilizes a repeating waveform for easier viewing and analysis. However, incorrect trigger settings can result in unstable or inconsistent displays, making it difficult to measure time intervals accurately.
- How to avoid: Familiarize yourself with the triggering options available on your oscilloscope. Make sure to set the trigger level and type (e.g., edge triggering, pulse triggering) appropriately for your specific measurement needs.
- Implications: Poor triggering can lead to "jittery" displays or even completely incorrect measurements, making it challenging to draw valid conclusions from your data.
Sampling Rate
The sampling rate defines how many samples the oscilloscope takes in a given period. If the rate is too low, the oscilloscope may not capture all the details of the waveform, leading to inaccuracies in your time interval measurements.
- How to avoid: Ensure that your oscilloscope's sampling rate is sufficient for the signals you’re analyzing. Typically, a sampling rate at least ten times higher than the frequency of your signal is recommended for a detailed representation.
- Implications: A low sampling rate can result in a phenomenon called aliasing, where higher-frequency components appear as lower-frequency artifacts. This can severely distort your understanding of the signal and your subsequent measurements.
By steering clear of these common mistakes, you improve the likelihood of obtaining accurate and reliable time interval measurements, ensuring that your data genuinely reflects the behavior of the systems you're studying.
Select up to 3 instruments to compare
Best Practices
Maximizing the accuracy of time interval measurements on an oscilloscope involves more than just avoiding common errors; it also requires adopting best practices.
Here are some quick yet impactful tips.
Calibrate Regularly
- Action: Stick to a regular calibration schedule using traceable standards.
- Benefit: Ensures consistent accuracy and early identification of potential issues.
Use Average Mode
- Action: Enable averaging for repetitive signals.
- Benefit: Reduces noise, improving measurement reliability.
Employ High-Resolution Mode
- Action: Activate high-resolution mode in your oscilloscope's settings.
- Benefit: Enhances vertical resolution and minimizes random noise.
By following these simple practices, you can significantly improve the precision of your time interval measurements.
Conclusion
Measuring time intervals accurately is a cornerstone skill for anyone working with oscilloscopes. Whether you're capturing single-shot or repetitive events, understanding key parameters like resolution, accuracy, and jitter is critical.
While several common mistakes, such as insufficient bandwidth or incorrect triggering, can compromise your measurements, adhering to best practices like regular calibration and employing high-resolution mode can significantly improve your results.
In the quest for impeccable time interval measurements, the quality and capabilities of your equipment can make all the difference.
If you're in the market for high-quality equipment that ensures optimal performance, look no further than Keysight Used Equipment Store.
We offer a wide range of premium used oscilloscopes, signal analyzers, waveform generators, multimeters and more that meet stringent quality standards. Upgrade your lab today for precision you can count on!
Whenever You’re Ready, Here Are
5 Ways We Can Help You
Browse our Premium Used Oscilloscopes,
Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri
Contact our sales support team
Create an account to get price alerts and access to exclusive waitlists
Talk to your account manager about your specific needs.