The new features and enhancements in PathWave Device Modeling 2023. The lesson covers a new Model Generator that enables one-click import of measured data, creation of trend plots, organization of the extraction flow, basic QA verification, and documentation. It also covers Python 3 support, integrated plotting, and linkage to customized installations. The lesson includes a hands-on exercise in which you will use the new Model Generator to generate a device model.