A transportable license behaves like a node-locked license but can be unlocked from one host and transported (moved) to another host. The steps to transport a license are summarized below or you can click the video for a demo. 

What is the Process for Transporting a License?

If a license is transportable, you can transport (move) it to a different host. The process to transport licenses is as follows:

  1. Deactivate the license on the host where it now resides.
  2. Connect to KSM and synchronize.
  3. Assign the license to the new host (provide the new host ID).
  4. Install the license (received from KSM) on the new host.