What Quantum Means for Aerospace Defense
Once a focus of sci-fi dreamers, quantum information technologies are now being targeted for their potential in real-world applications outside of R&D. Aerospace defense is one industry that stands to be greatly altered by quantum technologies. The advantages of quantum technologies range from better encryption and decryption for secured communications through improved detection of threats – either in code or by air, land, or sea. To prepare to leverage quantum in aerospace defense applications, it is best to gain an understanding of the current state of quantum technologies.
According to the Keysight University course, “Impact of Quantum Technologies on Aerospace Defense,” three main quantum technologies are being researched today:
- Quantum communications – the building of secure data pipelines through quantum cryptographic key distribution
- Quantum computing – data encryption including optimization of computational algorithms for modeling systems as well as big data and artificial intelligence
- Quantum sensing – extreme sensitivity for applications in terms of precision, timing, and navigation through methods like electromagnetic sensing
To understand quantum computing, it is essential to understand qubits. Classical computers perform tasks with billions of deterministic transistors, measured in 0s or 1s. For a quantum computer, information is defined by qubits. It scales exponentially, whereas classic systems scale linearly. Qubits are notable for their property of entanglement, which leads qubits to react to changes in other states instantaneously, over any distance. By measuring just one entangled qubit, you can deduce the properties of its partner as well.
Qubits are limited by quantum decoherence, which is the loss of information from the quantum system to the environment. Essentially, it places the qubit in an uncontrolled quantum state. It arises from imperfections in qubits, uncontrolled interactions with the environment, or errors in classical control. To avoid decoherence, you can increase system isolation from environmental defects, engineer control hardware and cabling for better qubit lifetime, and improve qubit materials. Preventing decoherence is critical to the realization of quantum computers.
This is just a small example of the immense knowledge to be gained around quantum technologies. In a world where spectrum dominance and technological superiority determine the winning side, aerospace defense agencies worldwide are prioritizing quantum for the vast improvements it will deliver. In recent years, most economic powers ramped up their quantum investment, with China and US investing billions. Japan, Germany, The Netherlands, India, and others also are investing more in quantum research, looking to speed development efforts. They recognize the advantages offered by quantum computing, sensing, and communications.
To solidify your understanding of quantum technologies and the role they will play in aerospace defense applications, register for our course.
Be sure to also check out our quantum solutions page for more resources.