power electronics trends in 2024

What’s Next for Power Electronics? Beyond Silicon

For more than half a century, silicon has been the bedrock of power electronics. Yet, as silicon meets its phy physical limitations in higher-power, higher-temperature applications, the industry’s relentless pursuit of more efficient power systems has ushered in the wide bandgap (WBG) semiconductors era. The global WBG semiconductors market reached $1.6 billion in 2022, with an estimated CAGR of 13% for the next 8-year period. The adoption of WBG semiconductors, notably silicon carbide (SiC) and gallium nitride (GaN), is now setting new benchmarks for performance in power systems across automotive, industrial, and energy sectors. What impact will WBG semiconductors have on power electronics (PE) trends in 2024, and how are they redefining the design and simulation workflows for the next decade?

Read 5 Critical PE Design Considerations for GaN

The catalyst for change: Wide bandgap

The term 'bandgap' refers to the energy difference between a material's insulating and conducting states, a critical factor determining its electrical conductivity.

As shown in Figure 1, with its wide bandgap, Gallium Nitride (GaN) exemplifies the three key advantages this property can offer.

Figure 1. Wide bandgap semiconductor properties

switching speed Gan and SiC

Figure 2. Switching speeds of SiC and GaN

GaN and other wide-bandgap semiconductors offer solutions for high-power, high-frequency, and high-temperature applications with improved energy efficiency and design flexibility.

Emerging challenges in power electronics simulation

The wider adoption of wide bandgap (WBG) semiconductors, including silicon carbide (SiC) and gallium nitride (GaN), sets new standards in the design of Switched Mode Power Supplies (SMPS) – power efficiency, compactness, and lighter weight.

However, the higher switching speeds of GaN and SiC demand more sophisticated design considerations. Power electronics engineers must manage electromagnetic interference (EMI) and optimize thermal performance to ensure reliability and functionality. Layout parasitics, for instance, can lead to voltage spikes in the presence of high di/dt values. Power electronics engineers face the following pressing questions.

To navigate these complexities, engineers need advanced simulation solutions to address layout parasitic effects effectively and come with robust thermal analysis.

advanced thermal analysis, PE design. SMPS design

Figure 3. Thermal analysis at board and schematic levels using Keysight’s PEPro

Key Impacts of WBG Semiconductors: From EVs to Renewable Energy

Electric vehicles (EVs)

As global EV sales are projected to increase by 21% in 2024, the power efficiency of automotive power electronics is paramount – every additional percentage is a big win. GaN enables more compact and efficient designs of onboard chargers and traction inverters, extending driving ranges by up to 6%.

Data centers

The digital economy's expansion brings a surge in data center energy consumption, with the U.S. expected to require an additional 39 gigawatts over the next five years—equivalent to powering around 32 million homes. Wideband semiconductors may be key to addressing this challenge by enabling higher server densities and reducing energy consumption and carbon emissions. Specifically, the implementation of GaN transistors in data center infrastructure can lead to a reduction of 100 metric tons of CO2 emissions for every 10 racks annually. This efficiency gain is particularly relevant as the computational and power demands of artificial intelligence (AI) applications soar, potentially tripling the racks’ power density.

Renewable energy

Wide bandgap semiconductors allow for more reliable power output and cost-effective solutions in both residential and commercial renewable energy storage systems. For instance, GaN transistors could achieve four times less power loss than traditional silicon-based power solutions.

The Road Ahead in the Era of WBG Semiconductors

GaN and SiC represent a new wave of material innovation to elevate the efficiencies of power electronics and redefine how we power our world. As the applications for WBG semiconductors expand, Keysight empowers our customers with a unified simulation environment to design reliable and long-lasting electronic systems under various operating conditions.

Are you curious about how WBG semiconductors will continue to transform power electronics? Meet us at APEC 2024, booth 1935, from Feb 25-29. Witness how our latest power electronics and power integrity solutions accelerate power electronics innovations, from EVs to renewable energy and beyond.

Request a demo

limit
3