Low-Frequency Noise Modeling

Low-Frequency Noise Modeling When Quantum Chips Are Getting Noiser

Since Richard Feynman first conceptualized the quantum computer in 1982, quantum computing has been the holy grail for scientists and researchers worldwide. With McKinsey predicting a quantum technology market of over $100 billion by 2040, the quantum arena is buzzing with over 350 startups pushing technological innovations and tech giants like IBM, Google, and Microsoft riding the quantum wave. Just a few months ago, Google built a quantum computer that could execute a task in 6.18 seconds that would conventionally take 47 years.

Amidst the headway, there is an imperative to navigate the challenges posed by noise – an inherent and spontaneous fluctuation in current or voltage – in quantum systems. Only by creating robust noise models can researchers predict their behavior to improve new hardware design and develop quantum error correction methods.

This article will delve into the importance of noise modeling for quantum computing, the challenges in low-frequency noise (LFN) measurement and explore how Keysight’s advanced low-frequency noise analyzer (A-LFNA) unlocks more accurate and efficient noise modeling for quantum computing.

Quantum Computing: Where Does Noise Come From

In the intricate quantum realm, computers, operating at cryogenic temperatures, rely on qubits to process massive amounts of data simultaneously.

A qubit must maintain quantum coherence to enable the creation and manipulation of superpositions. Yet quantum coherence is highly susceptible to external influences, including noise in the system. Even minor changes in environmental temperature and electrical or magnetic fields can cause the qubit to lose its coherence. As quantum computers grow in qubit count and the size of transistors shrinks, the complications from types of noise amplify. Let us delve into the primary contributors:

Electronics noise at low frequencies

Figure 1. Electronics noise at low frequencies

Of particular concern to quantum researchers is the low-frequency noise (LFN), also known as "1/f noise." This noise arises at frequencies below a device's typical operational frequency. As technological advancements push device size to shrink further, LFN variation goes up, making it more challenging to characterize. Today, there is a growing demand for robust LFN modeling for CMOS devices at cryogenic temperatures, particularly in the absence of a standard physics-based model.

This raises a pivotal question: How can quantum researchers untangle these complex noise challenges?

Confronting the Noise Measurement Challenges

To characterize noise that causes qubit decoherence, researchers need insights not only into the noise spectrum but also its statistics. By better understanding the underlying physical processes, researchers can effectively distinguish errors from the quantum system itself versus external sources. However, the exponentially growing noise characterization data, along with the sheer amount of time a typical 1/f noise measurement, is daunting. Additionally, a good measurement must take multiple samples and averaging, while as frequencies drop, sample times turn into minutes or longer.

So, how does a quantum engineer go about measuring noise, especially when the signals are quite small? How do they account for external factors, including the very equipment used for measurement, that can introduce further noise? How long can it take for measurements to stabilize?

Addressing these nuances necessitates on-wafer measurement. Rapid on-wafer measurement speed is important to develop an accurate device noise model since noise is random, and the statistical analysis of many device noises is necessary.

Key Steps for LFN Characterization and Modeling

Performing comprehensive low-frequency noise (LFN) modeling is key to improving the performance of quantum computers.

This involves a tight integration of experimental physics, data analysis, and modeling to understand and control the noise affecting quantum systems. The process encompasses:

  1. Identify the noise: The first step is to identify the origin of the LFN, which may stem from qubit frequency fluctuations, thermal vibrations of ions in the lattice, or magnetic flux variations.
  2. Measure the noise: Perform Ramsey Experiments to assess the frequency noise affecting qubit phases. Implement dynamical decoupling sequences (like Uhrig or CPMG) to suppress high-frequency noise further and focus on low-frequency characterization.
  3. Noise modeling: Apply Fourier Transform to the time-domain data obtained from experiments to extract the noise power spectral density (PSD).
  4. Analyzing data: Analyze the cross-correlation of noise affecting different qubits to understand spatial noise correlation. Develop theoretical models based on experimental data to describe the noise behavior.
  5. Validating the model: Fit the noise models to the experimental data and validate them with repeated independent experiments.

Keysight’s A-LFNA Solution: Automate the Full-wafer Level Characterization

At Keysight we envision an ideal low-frequency noise (LFN) measurement solution that would be accurate, efficient, work for all silicon devices, have a wide bandwidth, provide high resolution, cover a wide voltage range, be sensitive to low currents, and be easy to set up and use.

Eight considerations for choosing an LFN measurement solution

Figure 2. Eight considerations for choosing an LFN measurement solution

Our Advanced Low-Frequency Noise Analyzer (A-LFNA) is a turnkey solution to measure LFN for all types of CMOS devices. With its innovative noise sensitivity and tight integration with WaferPro Express, it is revolutionizing the way quantum engineers handle LFN measurements.

Advanced Low-Frequency Noise Analyzer

Figure 3. Keysight’s E4727B Advanced Low-Frequency Noise Analyzer (A-LFNA)

A-LFNA enables a closer look at noise in both the packaged and the wafer levels. A quantum engineer can leverage the A-LFNA’s industry-leading noise sensitivity (-185 dBV2/Hz) to characterize devices at hi-voltages (to 200 V) and down to ultra-low frequencies (to 30 mHz). In addition, Keysight’s close collaboration with FormFactor enables a complete integrated on-wafer solution with automated control of all major wafer probing systems.

Conclusion

In the age where quantum computing edges closer to practical reality, Keysight's A-LFNA is poised to guide the industry through complex noise modeling challenges, ensuring that the quantum computers of the future are both reliable and accurate.

Watch an on-demand seminar with FormFactor to hear from industry experts about how we help our customers navigate through the noisy channels toward more reliable, larger-scale quantum computers.

Keysight FomFactor integrated on-wafer solution for noise measurement

Request a free trial

limit
3