Bring new realism to NAVWAR testing with continuous dynamic range in PNT X
Radio frequency (RF) jamming is one of the most prevalent threats to navigation equipment, especially in navigation warfare (NAVWAR) scenarios. Developers of receiver equipment therefore want to know how, realistically, the receiver will respond to the presence of jamming interference.
In particular, developers often need to understand the impact on the receiver in dynamic scenarios where the device under test (DUT) is moving into or out of range of one or more high-powered jammers. However, reproducing such conditions realistically in the lab is tricky.
The need for a high dynamic range for realistic jamming scenarios
One issue lies with the need to simulate signals at very different power levels. Noise from a jammer can be many times louder than global navigation satellite system (GNSS) signals, which are typically -130 dBm at the receiver. This is particularly true of the high-powered jammers typically deployed by nation states.
Generating low-power GNSS signals and high-power jamming signals within the same simulator unit creates a technological challenge, however. There is a risk that very loud jammer noise may leak into the channels producing GNSS signals, affecting the reliability of test results.
Typically, this has meant that simulators have only been able to produce jamming signals in a restricted power range. While this can still provide valuable insights into receiver behavior, it represents a compromise in terms of test realism.
Keysight addresses this issue by placing GNSS signals and jamming waveforms on different radio cards, effectively isolating them from each other. Using this approach, the PNT X platform uniquely offers developers the ability to achieve very high jammer-to-signal (J/S) ratios within the same simulator unit: up to 150 dBm of difference between the jammer signal and the GNSS signal.
This allows even the most powerful jammers to be emulated realistically in the lab without requiring a separate interference generator and all of the complexity and cost that come with it.
Additionally, PNT X has slots for up to 10 radio cards, each with 64 channels of output. This means the simulator is capable of generating RF on up to 640 channels—ideal for testing mission-critical scenarios in complex RF environments with multiple jamming sources.
Continuous dynamic range in Keysight PNT X brings new realism to NAVWAR testing
Another consideration is that in real-world scenarios, the J/S ratio is usually not constant, but dynamic based on the position of the receiver relative to the jammer. In the case of an aircraft flying into a conflict zone, for example, jammer noise may start off quieter than the GNSS signal, get louder as the aircraft gets closer to the jammer, and tail off as the aircraft exits the jammer’s range.
In some conflict zones, there may be more than one jammer in the vicinity of the receiver at any given time. This creates a complex RF environment with rapidly-fluctuating jamming signals as the receiver moves through the zone. To reproduce these conditions accurately in the lab, the simulator needs to be capable of stimulating multiple, dynamic J/S ratios within a wide dB range.
To address this challenge, PNT X uniquely offers developers a continuous dynamic range of up to 140 dBm. This enables the power of the simulated jamming waveforms to fluctuate within a range starting from lower than GNSS at -130 dBm (producing a negative J/S ratio) to levels around the 0 dBm typical of the highest-power jammers.
While this is extremely difficult to achieve technologically, PNT X makes it possible by splitting the power range across separate radio cards, and switching seamlessly between them in test scenarios that require J/S ratios to fluctuate rapidly within a broad range.
Complementary features add further flexibility to interference scenarios
The continuous dynamic range in PNT X becomes especially powerful when used in conjunction with other capabilities of this simulator platform, including:
Inject custom I/Q files with SimIQ: The SimIQ tool enables custom waveforms to be injected as in-phase / quadrature (I/Q) files and upconverted to RF in the simulator. This allows developers to simulate custom or proprietary jamming signatures alongside GNSS and other positioning, navigation, and timing (PNT) signals — including from low Earth orbit (LEO) — within the platform.
Define multiple jammers with one I/Q file: The same I/Q file can also be used to define multiple independent transmitters, supporting NAVWAR scenarios featuring multiple jamming sources. Keysight’s spatial awarenessfeature automatically applies realistic effects like power levels, Doppler shift, and signal delay to I/Q-defined jammers during the test scenario.
Model realistic environments: The 3D terrain modelingfeature in PNT X enables developers to define the physical environment of the test scenario and place transmitters and receivers within it. The platform automatically applies effects such as multipath, signal obscuration, and signal diffraction to the signals and equipment under test, including to signals and waveforms generated from injected I/Q files, further increasing the realism of the test scenario.
PNT X: Unprecedented flexibility and realism in PNT vulnerabilities testing
Continuous dynamic range is just one of the many powerful features in PNT X, the world’s most advanced PNT simulator. PNT X brings unprecedented flexibility and realism to vulnerabilities testing, enabling more testing to be completed in the lab before moving to validation in a live environment.
To learn more about Keysight PNT X, visit the Keysight PNT X product page .