Impedance Analyzers | Keysight Equipment for Circuit Designers and Test Engineers

Why Your Circuit Designers and Test Engineers Need Impedance Analyzers


Key takeaways:

All engineers know resistance is usually bad news. It generates heat. It reduces efficiency. It wears out components and cuts operational lifetimes.

However, resistance is not the only kind of opposition to the current. When more complex waveforms are involved (like in radio applications), the inductors and capacitors contribute a different kind of opposition that is highly dynamic and complicated.

Impedance analyzers are the instruments of choice to understand this overall opposition to current flow. In this article, find out what impedance analyzers do, where they are used, how they work, and how to use them.

What is an impedance analyzer?

An impedance analyzer is an electronic test instrument that measures the characteristic complex impedance curves of a component, circuit, or material when subject to a range of alternating current (AC) signals.

Impedance, measured in Ohms (Ω), consists of two types of oppositions to the flow of alternating current: resistance and reactance.

Reactance is the opposition due to the inductances and capacitances of a material, component, or circuit. While resistance is not frequency-dependent, inductance, capacitance, and therefore reactance all vary with the frequency.

Because of this, the impedance is effectively a dynamic characteristic because its reactance varies with the signal frequency.

Impedance Analyzers | Impedance Is a Complex Quantity of Resistance and Reactance

Figure 1. Impedance is a complex quantity of resistance and reactance

The term "complex impedance" is used because it's mathematically convenient to represent it by a vector in a two-dimensional complex plane with a real axis (the resistance) and an imaginary axis (the reactance). The magnitude of this vector is the total impedance, while the direction tells us about the phase difference between voltage and current.

What are some applications of impedance analyzers in electronics and materials testing?

Impedance analysis is useful in multiple industries where the characterization of components, materials, and circuits under AC waveforms is essential. Various uses of impedance analyzers are outlined below.

Electronics

Analog circuits, like voltage-controlled oscillators, amplifiers, filters, and power supplies, and their components, like resonators and inductors, involve phenomena where impedance parameters like the resonant frequency and quality factor are sensitive to signal levels and frequencies.

Understanding their dynamic behaviors using analyzers with wide impedance ranges is crucial for optimum operational design and efficiency.

Telecommunications

Analyzers help achieve optimum impedancematching in antennas and transmission lines for signal transmission with maximum power transfer and minimal noise.

Additionally, cellular network components are optimized based on impedance measurements.

Power systems

Impedance analyzers are used to characterize devices like transformers and generators to minimize power losses. They are also used in renewable energy devices like solar inverters to optimize conversion efficiency and power quality.

Aerospace

Impedance analyzers are used to test and optimize communication links and navigation systems in aircraft and spacecraft.

Automotive

Impedance behaviors of batteries, battery management systems, and electronic control units are characterized for improving reliability, safety, and efficiency.

Material science

Impedance analyzers are widely used to study the electrical properties of conductive and semiconductive materials.

How does an impedance analyzer differ from an LCR meter?

Like impedance analyzers, inductance-capacitance-resistance meters (LCR meters) can also measure complex impedance. But their capabilities and usage are different, as listed below:

How do impedance analyzers work?

There are multiple techniques to measure unknown impedances, each with various pros and cons. The measurement hardware in impedance analyzers is designed to implement one of these techniques. The methods are outlined below.

Bridge method

Impedance Analyzers | Bridge Circuit Method Illustration(D Is the Instrument and Zx Is the Unknown Impedance)

Figure 2. Bridge circuit method (D is the instrument and Zx is the unknown impedance)

This traditional technique uses a simple bridge circuit to compare the unknown impedance with a known reference.

It's simple and effective for low-frequency measurements. However, it does not support high frequencies and very low impedance values.

Current-voltage (IV) method

Impedance Analyzers | Circuit for Current-Voltage Measurement Method

Figure 3. Circuit for current-voltage measurement method

A known voltage is applied to the circuit or component. The resulting current is then measured to calculate impedance.

This method is simple and versatile. However, the phase relationship between voltage and current must be correctly accounted for.

Radio frequency (RF) IV method

Radio Frequency (Rf) Iv Method | Circuits for Rf IV Method

Figure 4. Circuits for RF IV method

This technique extends the IV method to work accurately at the higher frequencies prevalent in RF circuits. It involves more sophisticated designs to accurately measure phase differences at these high frequencies.

Auto-balancing bridge method

Auto-Balancing Bridge Method Diagram Schematic

Figure 5. Auto-balancing bridge method

This method uses a feedback mechanism to automatically and dynamically balance the bridge circuit while the frequency is changing. It supports a very wide range of frequencies and impedances with high accuracy. However, its hardware design is more complex.

How do you use an impedance analyzer to measure the impedance of electronic components?

Impedance Analyzers | Impedance Analyzer Test Setup

Figure 6. Impedance analyzer test setup

The typical configuration for impedance analysis of individual electronic components includes:

How can an impedance analyzer be used to measure complex impedance in circuits?

For circuit designs, printed circuit boards (PCBs), and PCB assemblies (PCBAs) that operate exactly to specifications, the impedance characteristics of their circuit blocks and materials must be understood accurately.

These characteristics depend on the signal frequency, signal voltage, temperature, humidity, and similar operational factors. So, impedance analyzers are used as described below:

How do impedance analyzers contribute to the characterization of materials and sensors?

Device manufacturers must know the behaviors of the materials used in their wafers, semiconductors, and PCBs under actual operating conditions.

Impedance analyzers support relevant measurements like:

What frequency ranges are typically supported by impedance analyzers?

Impedance Analyzers | Impedance and Frequency Measurement Ranges of Different Designs for ±10% Accuracy

Figure 7. Impedance and frequency measurement ranges of different designs for ±10% accuracy

The measurement method used by a particular analyzer decides its supported frequency and impedance ranges as shown above and described below:

What factors should you consider when selecting an impedance analyzer for a specific application?

When selecting a suitable impedance analyzer, consider the following aspects.

How do temperature and environmental conditions affect impedance measurements using an analyzer?

It's critical to remember that impedance is highly dynamic. Environmental conditions like temperature, humidity, and electromagnetic interference (EMI) can drastically affect measurements, as described below:

Keysight impedance analyzers

Keysight's suite of high-accuracy impedance analyzers consists of three instruments with the following key features:

All these instruments support data export interfaces like the general purpose interface bus (GPIB), local area network (LAN), and universal serial bus (USB).

Overcome impedance with Keysight instruments

In this article, you learned about the uses of impedance analyzers and their key aspects.

Keysight'simpedance analyzers provide highly accurate impedance characterization for multiple industries and applications, from semiconductors to the largest power systems.

Contact us for insights and advice on selecting the right impedance analyzer for your lab or field tests.

limit
3