AI Data Center Fundamentals | AI Data Center Storage Center

AI Data Center Fundamentals: What It Is and How It Works


Almost every time you ask your favorite artificial intelligence (AI) chatbot a question, the request is processed by a specialized computing environment built for high-volume AI workloads.

It consists of thousands of servers, each with powerful purpose-built chips that perform massive numbers of parallel calculations. Helping those chips are several high-performance storage, memory, and networking technologies that make up an AI data center.

Below, we cover the technologies that power AI data centers, how they handle training and inference workloads, and why they've become the backbone of modern AI.

Key takeaways:

What is an AI data center?

An AI data center is a specialized computing facility designed to handle the enormous computational needs of AI workloads with low latency. It facilitates the full AI lifecycle of data ingestion, model training, fine-tuning, and real-time inference.

Unlike traditional data centers, AI data center infrastructure is more purpose-built and optimized for much higher performance.

For example, when you ask a chatbot a question or ask an AI service to fine-tune a large language model (LLM) on your custom data, that request is processed end-to-end by an AI data center.

What technologies are used in AI data centers?

AI Data Center Cluster Flow of Connections

Figure 1. AI data center

AI data center hardware relies on five specialized technologies to minimize latency across every layer of the stack:

  1. AI accelerators
  2. high-performance memory
  3. high-speed local and distributed storage
  4. high-bandwidth networking
  5. orchestration software and AI software frameworks

What are AI accelerators?

AI accelerators are specialized modules that can execute the mathematical and matrix operations of AI models at very high speeds. AI accelerators can deliver dramatically higher throughput than general-purpose CPUs for the highly parallel matrix and tensor operations common in AI workloads.

AI accelerators are the primary processors in AI data center servers. They’re supported by traditional CPUs, which handle system-level tasks, managing resource allocation, and orchestrating data pipelines. AI accelerators are typically deployed as PCIe cards, SXM/OAM-style modules, rack-scale systems, or specialized wafer-scale systems — consisting of:

Examples of popular AI accelerators include:

Which high-performance memories are used in AI data centers?

Memory technologies preferred in AI data centers include:

AI accelerators run at such high speeds that traditional memory becomes a bottleneck. Keeping the compute cores constantly fed with data is a significant challenge. The above technologies alleviate this memory wall in different ways.

HBM3E provides extremely high memory bandwidth, with implementations reaching approximately 1.2 TB/s per stack. An accelerator typically combines multiple HBM stacks to achieve several terabytes per second of aggregate memory bandwidth.

CXL enables CPU‑side memory pooling and expansion, improving memory capacity for inference‑heavy or heterogeneous workloads.

What storage technologies are used in AI data centers?

AI data centers prefer high-speed non-volatile memory express (NVMe) solid-state drives and storage architectures built upon NVMe-over-fabrics (NVMe-oF), GPUDirect Storage, and parallel file systems.

Both the capacity and speed of AI data center storage are critical. It must store large training and inference datasets as well as potentially numerous model checkpoints and associated training state. It must also fetch all this data at high speeds to avoid bottlenecking the ultra-fast AI accelerators.

NVMe-oF extends NVMe storage access across a high-performance network, enabling compute nodes to access shared or disaggregated NVMe storage with high bandwidth and low latency.

GPUDirect Storage enables direct DMA transfers between storage and GPU memory, avoiding the traditional CPU-memory bounce buffer and reducing CPU overhead.

Scale-out parallel file systems and object stores provide data management for these storage technologies.

Which networking technologies are used in AI data centers?

AI Data Center Networking Technologies | AI Data Center Networking

Figure 2. AI data center networking

AI data centers rely on high-performance networking technologies including InfiniBand and Ethernet-based fabrics.

InfiniBand is a networking technology designed explicitly for high-performance computing and AI. It's an alternative to Ethernet-based fabrics and relies on tightly integrated, purpose-specific hardware.

Modern AI Ethernet fabrics commonly support RDMA using RoCEv2 (RDMA over converged Ethernet). RoCEv2 brings the benefits of RDMA to standard Ethernet networks by enabling RDMA over routable IP networks. It is commonly deployed with lossless or loss-managed Ethernet techniques such as Priority Flow Control (PFC), Explicit Congestion Notification (ECN), and Data Center Quantized Congestion Notification (DCQCN).

High-bandwidth Ethernet, scaling up toward 800G, 1.6T, and beyond using optical fiber, is an essential backbone of AI data center networking.

Which software is used in AI data centers?

AI data centers rely on software for cluster orchestration, distributed model inference, model serving, and distributed model training.

These software stacks orchestrate the hardware resources and software components needed for model training and inference. They operate across multiple layers, from foundational communication libraries up to high-level workload orchestrators.

Cluster orchestration software manages containers, container resources (compute, memory, storage, and network), task scheduling, and fault tolerance. Popular solutions include Kubernetes, Anyscale Ray, Slurm, and their cloud-based versions.

Distributed model inference and serving stacks offer AI models and their inference capabilities through application programming interfaces. Hyperscalers and AI service providers, such as Google Cloud, OpenAI, Microsoft, and Anthropic, use proprietary inference engines to handle their hyperscale workloads. Other service providers may use open-source inference engines like vLLM.

Distributed model training stacks are needed to orchestrate training of large models, which requires high computational power and is very data-intensive. These stacks reduce training times by distributing tasks using frameworks such as DeepSpeed, PyTorch Distributed, and the NVIDIA Collective Communications Library.

How do AI data centers work?

The technologies in AI data centers interact differently depending on the training or inference stage of an AI workload lifecycle, as explained below.

How do AI data centers work during model training?

During AI training or fine-tuning, all the layers of AI infrastructure — compute, storage, interconnects, memory, and networks — face intense loads for extended periods.

The steps and loads are outlined below:

How do AI data centers work during model inference?

Compared with training, an individual inference request typically performs less computation because it runs a forward pass through an already-trained model. But production inference can place enormous pressure on AI data centers. At scale, serving thousands or millions of concurrent users requires careful management of GPU memory, KV cache, batching, network traffic, tail latency, and cost per token. The steps during model inference are as follows:

How is an AI data center different from a traditional data center?

An AI data center differs from a traditional enterprise data center in its architecture, workload, power, and cooling.

How is AI data center architecture different from an enterprise data center?

AI data center architectures use different compute, network, interconnect, storage, and memory technologies than traditional data centers.

Compute type
GPU or TPU dense
CPU centric
Processors

NVIDIA GPUs

Google TPUs

Amazon Trainium

Cerebras Wafer Scale Engine

Intel Xeon

AMD EPYC

Virtualization / Containerization
Often deployed on bare-metal or highly optimized virtualized infrastructure to provide efficient access to accelerator resources.
Highly virtualized or containerized
Compute node allocation
Model characteristics, accelerator memory, parallelism strategy, and workload requirements influence how compute resources are allocated.
Many enterprise workloads are more loosely coupled and easier to schedule across generalized compute pools.
Network topology
"East-West" focus (server-to-server) through InfiniBand or RoCEv2 fabrics
"North-South" focus (server-to-internet) with standard TCP/IP routing
Interconnects
High-performance intra-server interconnects like NVLink or UALink
Standard interfaces like PCIe
Memory technologies

HBM

CXL

Error correcting code (ECC) double data rate (DDR4 / DDR5)
File system
Highly parallel file system
Regular network file system

How do AI workloads differ from typical enterprise workloads?

AI workloads include training, fine-tuning, inference, embedding generation, retrieval, data preprocessing, evaluation, and monitoring.

Large-scale AI training and inference can require hundreds or thousands of accelerators operating in parallel:

In contrast, enterprise workload tasks span many task types:

An enterprise data center may host millions of discrete, independent, diverse tasks.

How are power consumption and cooling different in AI data centers?

An AI data center has much higher power consumption and cooling requirements due to AI accelerator chips. As a result, AI data center energy efficiency has become a core design priority, driving investment in liquid systems, power delivery architecture, and chip-level thermal management.

Rack power density (industry ranges)
AI racks can reach power densities far beyond those common in traditional enterprise deployments, with leading accelerator systems driving rack-level power into the tens or even 100+ kW range.
Typically under 10 kW per cabinet
Cooling systems
Advanced liquid cooling is increasingly utilized due to the intense heat generated by AI accelerators

Direct liquid cooling circulates coolant through cold plates attached to high-power components such as GPUs and CPUs.

Traditional air conditioning

Raised floor cooling

Why are AI data centers essential for modern AI?

AI data centers are essential prerequisites to maintain the current trajectories of generative AI, AI agents, and enterprise ML adoption. Without continued advances in AI data-center infrastructure, the cost, performance, scalability, and latency requirements of increasingly capable AI workloads would become increasingly difficult to meet.

What role do AI data centers play in generative AI and LLMs?

The scalability and performance ofAI data centers are essential for training better LLMs and more powerful multimodal AI models.

Research has demonstrated predictable relationships between model size, training data, compute, and model performance. AI data-center infrastructure provides the compute, memory, storage, and networking required to scale these resources efficiently.

Training large-scale foundation models involves orchestrating thousands of GPUs or TPUs operating continuously for weeks to months. AI data centers are designed to sustain this level of synchronized computation without systemic failures or downtime, through resilient RDMA fabrics, distributed NVMe storage, and deterministic job schedulers.

Why are AI data centers critical for enterprise AI adoption?

AI data centers are critical to enterprises. To support large numbers of concurrent users, AI infrastructure must provide scalable inference with high concurrency, low latency, stable tail latency, and high throughput.

Enterprise adoption is crucial for better AI-powered business automation, more insightful analytics, machine learning, and generative AI workflows in critical sectors like:

AI data centers are the robust infrastructure backbones needed to effectively and profitably commercialize AI applications.

What scaling challenges come next for AI data centers?

KAI Data Center Builder | AI Data Center Network Scaling Flow Illustration

Figure 3. AI infrastructure hierarchy from chiplets to the network’s edge

AI data centers are crucial for ensuring future advances in AI capabilities and hardware. The adoption of advanced AI across enterprises and research environments depends on further optimizing these facilities for peak performance.

However, scaling up poses many challenges for AI data center design and testing. Energy grids have to scale up to supply power. High energy consumption, cooling demand, energy efficiency, sustainability, renewable energy sources, and environmental impact remain significant challenges. More powerful AI chips and interconnects are also needed.

Read more about these challenges of designing and testing AI data center infrastructure.

Rely on Keysight for AI data center validation

This article introduced AI data center technologies and how they work during typical AI tasks. Keysight products help engineers design, test, and validate every hardware and software layer of the next-generation AI data center.

Contact us for insights into AI data center design and testing.

limit
3
What is an AI data center?
An AI data center is a specialized computing facility designed to handle the enormous computational needs of AI workloads with low latency. It facilitates the full AI lifecycle of data ingestion, model training, fine-tuning, and real-time inference.
What technologies are used in AI data centers?

AI data center hardware relies on five specialized technologies to minimize latency across every layer of the stack:

  1. AI accelerators
  2. high-performance memory
  3. high-speed local and distributed storage
  4. high-bandwidth networking
  5. orchestration software and AI software frameworks
What are AI accelerators?
AI accelerators are specialized modules that can execute the mathematical and matrix operations of AI models at very high speeds. AI accelerators can deliver dramatically higher throughput than general-purpose CPUs for the highly parallel matrix and tensor operations common in AI workloads.
What storage technologies are used in AI data centers?

AI data centers prefer high-speed non-volatile memory express (NVMe) solid-state drives and storage architectures built upon NVMe-over-fabrics (NVMe-oF), GPUDirect Storage, and parallel file systems.

Both the capacity and speed of AI data center storage are critical. It must store large training and inference datasets as well as potentially numerous model checkpoints and associated training state. It must also fetch all this data at high speeds to avoid bottlenecking the ultra-fast AI accelerators.

Which networking technologies are used in AI data centers?

AI data centers rely on remote direct memory access (RDMA) technologies such as InfiniBand, RDMA over converged Ethernet (RoCEv2), and high-bandwidth Ethernet.

InfiniBand is a specialized networking technology designed explicitly for high-performance computing and AI. It's an alternative to Ethernet-based fabrics and relies on tightly integrated, purpose-specific hardware.

RoCEv2 brings the benefits of RDMA to standard Ethernet networks by enabling RDMA over routable IP networks. It is commonly deployed with lossless or loss-managed Ethernet techniques such as Priority Flow Control (PFC), Explicit Congestion Notification (ECN), and Data Center Quantized Congestion Notification (DCQCN).

High-bandwidth Ethernet, scaling up toward 800G, 1.6T, and beyond using optical fiber, is an essential backbone of AI data center networking.

Which software is used in AI data centers?

AI data centers rely on software for cluster orchestration, distributed model inference, model serving, and distributed model training.

These software stacks orchestrate the hardware resources and software components needed for model training and inference. They operate across multiple layers, from foundational communication libraries up to high-level workload orchestrators.

How do AI data centers work during model inference?
Compared with training, an individual inference request typically performs less computation because it runs a forward pass through an already-trained model. But production inference can place enormous pressure on AI data centers. At scale, serving thousands or millions of concurrent users requires careful management of GPU memory, KV cache, batching, network traffic, tail latency, and cost per token
How is an AI data center different from a traditional data center?
An AI data center differs from a traditional enterprise data center in its architecture, workload, power, and cooling.
How is AI data center architecture different from an enterprise data center?
AI data center architectures use different compute, network, interconnect, storage, and memory technologies than traditional data centers.
How do AI workloads differ from typical enterprise workloads?
AI workloads include training, fine-tuning, inference, embedding generation, retrieval, data preprocessing, evaluation, and monitoring.
How are power consumption and cooling different in AI data centers?
An AI data center has much higher power consumption and cooling requirements due to AI accelerator chips. As a result, AI data center energy efficiency has become a core design priority, driving investment in liquid systems, power delivery architecture, and chip-level thermal management.
Why are AI data centers essential for modern AI?
AI data centers are essential prerequisites to maintain the current trajectories of generative AI, AI agents, and enterprise ML adoption. Without AI data centers, these trends would hit a hardware wall, resulting in unacceptable latency.
What role do AI data centers play in generative AI and LLMs?

The scalability and performance ofAI data centers are essential for training better LLMs and more powerful multimodal AI models.

Research has demonstrated predictable relationships between model size, training data, compute, and model performance. AI data-center infrastructure provides the compute, memory, storage, and networking required to scale these resources efficiently.

Why are AI data centers critical for enterprise AI adoption?
AI data centers are critical to enterprises. To support large numbers of concurrent users, AI infrastructure must provide scalable inference with high concurrency, low latency, stable tail latency, and high throughput.
What scaling challenges come next for AI data centers?

AI data centers are crucial for ensuring future advances in AI capabilities and hardware. The adoption of advanced AI across enterprises and research environments depends on further optimizing these facilities for peak performance.

However, scaling up poses many challenges for AI data center design and testing. Energy grids have to scale up to supply power. High energy consumption, cooling demand, energy efficiency, sustainability, renewable energy sources, and environmental impact remain significant challenges. More powerful AI chips and interconnects are also needed.