The Inference Stack Can Talk — And We Can Learn a Lot by Listening
Inference systems — especially for teams building them for the first time (which increasingly includes many of us) — are often treated as high-performance black boxes. Prompts go in, tokens come out, and everything beneath the surface feels hidden behind layers of GPU, memory, network, scheduling, and orchestration. But the inference stack is far from silent. It communicates constantly through shifts in token latency, decode cadence, GPU utilization patterns, KV-cache expansion, and network behavior. Each of these signals is a message about how the system operates and what it responds to.
As we peek inside the inference systems, one thing became clear: if we listen intently, the stack reveals a lot — insights about workload balance, memory pressure, scheduling behavior, thermal boundaries, and both its comfort zones and breaking points. None of these signals indicate failure outright (at least not most of the time); rather, they highlight opportunities to optimize the system, so it performs better for your specific purpose.
It's a language we all must learn. Because if we listen carefully, the stack stops being a mystery and starts becoming a guide
What Exactly Can the Stack Say? A Lot, Actually
Inference telemetry can be considered a unified language. Its signals are not random fluctuations; they are precise, interpretable messages about how workloads interact with inference hardware and software. Below are a few simple but important examples of “voices” of the stack, followed by a set of honorable mentions that further enrich its vocabulary.
Prefill Spikes: “I am not able to compute fast enough”
Large prompts, long documents, and Retrieval Augmented Generation (RAG)-assembled contexts trigger heavy attention operations. When first token latency (Time to First Token-TTFT) rises or context processing slows, the stack says your workload is compute-bound during prefill and shows exactly where the pressure originates:
- “Your attention layers are running at full width.”
- “Tensor cores and Streaming Multiprocessor (SM) Cores are saturated with large context matrices.”
- “High Bandwidth Memory (HBM) bandwidth is being consumed and released aggressively.”
Telemetry reveals:
- High tensor utilization
- High SM occupancy and SM utilization
- Large spikes in memory write throughput
Decode Slowdown: “Large responses are filling up my memory”
During long-generation tasks or periods of high concurrency, the decode token cadence often begins to wobble. In those moments, the stack is signaling that its memory path is becoming overwhelmed — juggling constant reads of model weights and prompt context while simultaneously writing and maintaining KV-cache and RAM state. It is no longer compute-bound; it is memory-bound, and the slowdown in decode performance (the system’s ability to produce tokens consistently and respond quickly) reflects this shift.
- “I can generate tokens, but memory bandwidth is tightening.”
- “KV-cache lookups are growing expensive.”
- “Precision, concurrency, and output length are shaping token rate.”
Telemetry reveals:
- Time Per Output Token (TPOT) increases
- Lower tensor utilization; underfed GPUs
- Increased Inter-Token Latencies (ITL), Time to Last Token (TTLT)
KV-Cache Expansion: “I am struggling to remember ALL the past history”
As sessions grow longer — multi-turn chats, agents, long-context queries — the KV-cache expands substantially. The stack is saying your workload is state-heavy and showing how that state manifests internally:
- “Your conversation is persistent, and I’m storing it all.”
- “Longer sessions reshape my memory footprint.”
- “My responses will be slower as I have a large cache to refer from.”
Telemetry reveals:
- Steady increase in cache utilization
- Possible underutilization of GPU and HBM
- Continuously rising latency over extended sessions
Tail-Latency Wobble: “I am having trouble handling these sudden bursts”
When P99 inflates while P50 remains normal, the scheduler is clearly saying your system is burst-sensitive and explaining when and why tail latency appears:
- “Your arrival rate is exceeding my drain capacity.”
- “Concurrency is stretching my scheduling boundaries.”
- “Queue depth is amplifying latency for certain users.”
Telemetry reveals:
- Growing wait queues
- Load imbalance
- Variance between median Inter Token Latency and Time to Last Token’s P99, P90, P50 variances
Honorable Mentions
Inefficient Pipeline: “Your software is slowing me down”
Low utilization and irregular token flow often indicate that the pipeline, not the model or hardware, is the limiting factor. Things like poor batching strategy and unnecessary serialization underfeed the GPUs and create avoidable stalls.
RAG Fabric Jitter: “Your retrieval path is causing longer delays”
Round Trip Time (RTT) instability, storage I/O variance, and fabric delays show that retrieval topology directly affects prefill timing.
Power or Clock Throttling: “It’s hot in here and I don’t like it”
Thermal limits or power capping constrict GPU clocks and change throughput predictability.
Inter-GPU Communication Delays: “The GPUs aren’t getting along, and are having trouble working together”
Interconnect latency shapes multi-GPU efficiency; your networking might be slower.
The Stack Will Tell You Everything — But You Need to Make it Talk
Recognizing that the inference stack speaks is only half the equation. The other half is giving it the right reason (workload) to speak. An inference stack reacts to the workload placed in front of it, revealing the exact stresses, limits, and sensitivities triggered by that workload. But this communication only becomes meaningful when the workload reflects your true purpose, use case, traffic shape, concurrency profile, and operational reality.
In other words, the stack can tell you everything you need to know, but only if you make it talk in the context you care about.
Doing that requires two things:
- Purpose-aligned prompts at scale that recreate the exact shape of your usage.
- Unified observability so you can correlate what you sent with how the stack responded.
- Reproducibility that consistently replicates identical workload patterns to validate system behavior before and after fixes.
Keysight AI (KAI) Inference Builder Delivers on Both
KAI Inference Builder emulates a broad, curated library of prompt models and workloads that reflect real-world usage patterns across industries and application types. These aren’t synthetic or generic. They are purpose-engineered prompt shapes built from Keysight’s application research, threat intelligence insights, and cross-domain testing expertise. The library includes industry-specific workloads such as those seen in AI models at law firms, financial institutions, universities, healthcare providers, and more. It also includes technology-focused prompt suites for exercising specific inference components like model and pipeline behavior, GPU-cluster characteristics, storage access, memory, and KV-cache sensitivity.
KAI-IB Pairs Workload and Telemetry in a Single Pane of Glass
Even if the stack speaks, its insight is missing the big picture, if the signals are scattered across dashboards, logs, and tools. KAI Inference Builder solves this by presenting workload metadata, inference-engine-level telemetry (e.g., VLLM stats), and system-level GPU telemetry (e.g., data center GPU modeling and DCGM data) together in one synchronized view:
- Prompt shape and send rate
- Prefill/decode time
- Token timing (TTFT, TPOT, TTLT)
- GPU utilization
- Memory stats
- KV-cache growth and queue growth
- Latency curves
- Concurrent session load
- GPU Power stats
- Pipeline and scheduler behavior
All metrics are aligned, time-correlated, and immediately actionable. This matters because correlation is everything. With KAI Inference Builder, you see not just that something happened, but why it happened — and what the stack is signaling to improve.
Summary: KAI Inference Builder Turns the Inference Stack into an Advisor
By giving the inference stack the right prompt shapes and interpreting its responses through unified, time-aligned telemetry, KAI Inference Builder transforms the system from a black box into a collaborative partner — one that clearly communicates what it needs to perform at its best.
As KAI Inference Builder generates purpose-built workloads and its dashboard translates the resulting signals, the stack begins to articulate its requirements with clarity: that it needs more memory for certain workloads, that the scheduler struggles with specific concurrency curves, that network paths are decode-heavy prompts, that GPUs are being underfed, that thermal envelopes are prefill and shaping decode rates, or that prompt structures directly influence how layers execute.
This tool goes beyond examining inference stack internals; it emulates the full, authentic user experience — including network overhead and real-world interaction patterns — by measuring the entire end-to-end lifecycle rather than isolated components, delivering actionable insights at the stack level.