Consider Adding a Pre-Charge Step to Your Lithium-Ion Cell Manufacturing Process

Last year I posted an article “The ABCs of Lithium-Ion Cell Manufacturing” (click on title to access) that provides an overview of the lithium-ion cell manufacturing process. In my article I walked through 10 main steps of the manufacturing process, starting with preparing the materials that go into the cell’s construction and ending with final testing and grading. While these 10-steps are comprehensive, manufacturers are always looking at ways to enhance their process to better suit their specific needs. One way to consider enhancing the cell manufacturing process is adding a pre-charge step, as illustrated in Figure 1. As shown, pre-charge is a step that takes place before formation.


Figure 1: Adding a pre-charge step to the lithium-ion cell manufacturing process

What is pre-charge? Why add it into the manufacturing process?
Traditionally, after the cell is assembled and filled with electrolyte, the formation step then adds electrical charge to the cell, taking typically on the order of a day to perform. A portion of this charge is consumed to form the solid electrolyte interface layer (or SEI layer) on the surface of the cell’s anode. Hence the term formation. A properly formed SEI layer is paramount to a cell’s performance and long-term life. Additional electrical charge applied is stored as energy in the cell.

A lithium-ion cell’s state of charge (SoC) characteristic is depicted in Figure 2. As expected, the cell’s voltage varies with its % SoC. For this lithium ion cell type, the voltage is at 4.2 volts for 100% SoC (fully charged) and drops down to 2.5 volts for 0% SoC (fully discharged). This is not to say there is no charge left in the cell at 0% SoC, as there is a slight amount left. Instead, 0% SoC is defined by the minimum voltage level that the cell can remain at without risk of causing damage. Over-discharging the cell below its minimum voltage can cause internal corrosion and irreversible damage. This makes the cell potentially dangerous to recharge again.

After the step of filling a cell with electrolyte, it becomes electro-chemically active but still does not have any charge. Some time is allotted for the electrolyte to fully soak into the porous active materials of the electrodes, referred to as wetting. After this time however, the filled but uncharged cell may be sitting somewhere near 0 volts and subject to start corroding internally. It is imperative to apply some charge to the cell at this point to prevent this internal corroding from starting. Not enough charge to start forming the SEI layer or charge the cell, but just enough to “pre-charge” the cell to get it up to 2 to 3 volts, to prevent internal corrosion caused by too low of a cell voltage.


Figure 2: One type of lithium ion cell discharge characteristic.

Normally all the cells need to move immediately to formation after filling and wetting to prevent internal corrosion from starting, but this may not be the ideal situation for several reasons:

Adding a pre-charge step before formation may be a better alternative. Pre-charge consists of setting up stations like formation, but with differences:

Pre-charge can provide greater flexibility in the manufacturing process. There is no longer the immediate need to put all the cells through formation after electrolyte filling and wetting. This can provide greater flexibility in scheduling, putting the pre-charged cells through formation when it is opportune to do so.

Using the Keysight BT2200 Charge-Discharge System for Pre-charge:
The Keysight BT2200 Charge-Discharge System is well suited for both pre-charge and formation. The BT2202A or BT2203B mainframe, along with eight BT2204B modules provides 256 6-amp channels. For formation these channels can be connected in parallel for higher power and current as required, depending on the cell size. Individual channels are well suited for applying lower voltage and current typically required for pre-charge. The BT2200 also incorporates other specific capabilities uniquely needed for pre-charge, including operation down to or below 0 volts and short charge cycles, among other things. A BT2200 mainframe and BT2204B modules are pictured in Figure 3. More information about the BT2200 can be found by accessing the following: “Keysight BT2200 Charge-Discharge System product page”.


Figure 3: Keysight BT2200 Mainframe with BT2204B modules

To learn more about pre-charge:
A colleague of mine, Bob Zollo, who is a Solution Architect for battery test solutions for Keysight’s Electronic Industrial Solutions Group, has written an article “Pre-charging vs. Formation in Lithium-Ion Cells”. As well as serving as a reference for me for this posting, I strongly encourage readers here to review Bob’s article as well. It provides additional insights on what pre-charging is all about in lithium-ion cell manufacturing. Just click on the title to review!\

limit
3