Technical Overviews
Keysight Technologies
Compatibility and Differences:
34465A and 34410A/34411A/L4411A
Digital Multimeters
Technical Overview
The Keysight 34465A Truevolt digital multimeter (DMM) is the next-generation DMM for users that own the Keysight 34410A, 34411A, or L4411A. The new Truevolt DMM was designed by the same group that designed the previous generation of DMMs, with many of the same R&D engineers participating. With this continuity of experience and expertise, Keysight has made a DMM that is a virtual drop-in replacement for the 34410A or 34411A while continuing to evolve usability and measurement technology.
The 34465A is designed to be a compatible 34410A and 34411A replacement with few exceptions. If you are looking to migrate from the 34410A or 34411A to a 34465A and want to fully understand all differences between the two generations of DMM models, this application note will help you. The L4411A does not have a 1U direct replacement; however, you can achieve the same functionality and measurement capability with the Truevolt Series DMM. Our goal is to help you migrate from your current DMM to a Truevolt DMM effortlessly.
Compatibility
There are many factors when looking to replace reliable instruments such as the 34410A/34411A. Here are just some of the areas where the 34465A is equivalent with the older generation of DMMs.
Differences
The few differences between the 34465A and 34410A/34411A/L4411A DMMs that might affect migration are listed below. Many of these differences improve the performance of the 34465A relative to the 34410A/34411A models.
Physical differences
Calibration Differences
The 34465A and 34410A/34411A/L4411A use different calibration procedures, with different default passwords
Key measurement differences:
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.