Flyers
Keysight Technologies
Top 5 Reasons FieldFox is Your Ideal Cable and Antenna/Line Sweep Tester
For Wireless Installation and Maintenance
Your challenge
Fifty to sixty percent of cell site problems are caused by faulty cables, connectors, and antennas. As you know, degraded feed lines cause poor coverage, unnecessary handovers, paging failures, and access failures on the uplink. To avoid service quality problems, it is critical you have a reliable cable and antenna (CAT) analyzer to keep your cell sites’ systems in good condition. Until now, it has been challenging finding a tool that provides reliable and repeatable test results in varying environments and weather conditions.
Your solution
FieldFox handheld analyzers are rugged and portable RF and microwave analyzers that incorporate the same measurement science as many of the Keysight Technologies, Inc. high-performance benchtop instruments. FieldFox is a multi-function tool that enables you to handle wider frequencies, from the cellular to microwave bands, as well as different antenna and feeder-line configurations – whether it is a macro site, indoor DAS (distributed antenna systems) or outdoor DAS.
1. Rugged enough to meet MIL-specs
2. Display designed for use in direct sunlight
3. Make quick and accurate line sweep measurements in the field without a cal kit
Each instrument is CalReady at the RF Out port, immediately following power-on or preset. This means it’s already calibrated and ready to make measurements such as one-port cable loss, VSWR, return loss, and DTF measurements at the test port.
Industry’s first and only QuickCal: With traditional test instruments, you need to calibrate using a calibration kit (cal kit) when you add an additional device to the test port, such as a jumper cable or adapter. FieldFox provides the industry’s first and only built-in calibration system called QuickCal, which allows you to calibrate without the hassle of carrying a cal kit, and provides worry-free accuracy every time.
Broadband calibration: FieldFox allows you to make broadband calibrations, which means the instrument is calibrated over the maximum frequency span. After a broadband calibration, you can change the frequency range or number of points without recalibrating the instrument.
FieldFox provides the most comprehensive calibration techniques in the market place, and also supports OSL T cal, waveguide calibration and external ECAL.
4. Easily save, transfer and manage files
5. Future-proof with flexible upgradability
The base FieldFox analyzer is a fully functional cable and antenna tester – which means no extra options are needed to put your team to work. However, if your tasks change in the future, you can easily upgrade FieldFox with simple software license keys with the following functions: spectrum analyzer, power meter, interference analyzer, insertion loss measurement, full-2 port vector network analyzer, GPS, DC power supply and more – all without sending the unit back to Keysight for the upgrade.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.