Choose a country or area to see content specific to your location
Application Notes
The first popular standards for wireless LAN (IEEE 802.11a and b) were designed primarily to serve the needs of a laptop PC in the home and office, and later to allow connectivity “on the road” in airports, hotels, Internet cafes, and shopping malls. Their main function was to provide a link to a wired broadband connection for Web browsing and email. Since the speed of the broadband connection was the limiting factor, a relatively low-speed wireless connection was sufficient—802.11a provided up to 54 Mb/s at 5 GHz, and 802.11b up to 11 Mb/s at 2.4 GHz, both in unlicensed spectrum bands. To minimize interference from other equipment, both used forms of spread-spectrum transmission and were heavily encoded. A later revision of the standard, 802.11g in 2003, consolidated use in the 2.4 GHz band but maintained the maximum data rate at 54 Mb/s. However, by the same time, new usage models with the need for higher throughput had been recognized: data sharing amongst connected devices in the home or small office and wireless printing as examples. A study project was set up which produced 802.11n in 2009. As well as improving the maximum single-channel data rate to over 100 Mb/s, this new standard introduced MIMO (multiple input, multiple output) sometimes referred to as spatial streaming, where up to 4 separate physical transmit and receive antennas carry independent data that is aggregated in the modulation/demodulation process.
Unlock Content
Sign up for free
*Indicates required field
Thank you.
Your form has been successfully submitted.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.