Data Sheets
Keysight Technologies, Inc. oscilloscope automotive options help electronic system designers test and debug the physical layer of automotive serial buses faster. CAN, LIN and FlexRay serial buses are the backbone for communication among many separate controllers, sensors, actuators, and ECUs located throughout automotive and industrial designs. These serial bus interfaces provide content rich points for debug and test. However, since these protocols transfer bits serially, using a traditional oscilloscope has limitations.
Manually converting captured 1’s and 0’s to protocol requires significant effort, can’t be done in real-time, and includes potential for human error. Also, traditional oscilloscope triggers are not sufficient for specifying protocol-level conditions. Extend your oscilloscope capability with Keysight’s CAN, LIN and FlexRay protocol triggering and decode application.
This application makes it easy to debug and test designs that include these buses using your Infiniium oscilloscope.
CAN, LIN and FlexRay setup and protocol triggering
Get access to a rich set of integrated software protocol-level triggers. The application includes a suite of configurable protocol-level trigger conditions specific to CAN, LIN, and FlexRay. When serial triggering is selected, the application uses software-based triggering. With software-based protocol triggering, the oscilloscope takes signals acquired using either scope or digital channels and reconstructs protocol frames after each acquisition. It then inspects these protocol frames against specified protocol-level trigger conditions and triggers when the condition is met. Quickly move between physical and CAN protocol layer information using the time-correlated tracing marker. Display protocol content using embedded decode in the waveform area. Or, see protocol events in a compact listing format. For CAN minor tick marks indicate clock transitions. Major tick marks indicate segments of the serial packet such as ID, DLC, CRC, CAN measurements are automatically time-correlated with measurement on other scope channels. Import industry-standard .dbc files for symbolic triggering and decode. Message and signal values are displayed on the lister and in the waveform in symbolic format, making it easier to understand the oscilloscope capture. Long time captures using segmented memory In this example, CAN traffic was captured for near 35 seconds. Segmented memory uses time tags to track time between segment acquisitions
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.