Technische Überblicke
Many factors will define the evolution and adoption of commercial wireless technology. From the huge range of possible outcomes, it is useful to consider which factors are most relevant in predicting the future. Figure 1 shows the evolution of wireless since the start of the digital era in the early 1990s.
Much industry speculation and debate exists attempting to predict the next-generation market winners with the focus often being on the peak data rates possible. To take a more complete view, however, other important criteria should also be considered:
This article will examine the continuing growth in peak data rates and consider implications on achievable data densities, system cost and customer QoE. The issue of interference and the growing gap between peak and average data rates will be considered.
Over the last 20 years, mobile wireless systems have evolved from expensive, low-tech niche markets into one of the world’s biggest high-tech industries. Subscriber numbers this year will exceed 3 billion — or half the planet — with more to come. In addition to subscriber growth, Table 1 shows a parallel growth in cellular peak data rates of four orders of magnitude.
At this point, it would not be unreasonable to conclude that Moore’s law was predicting this growth in data rates, although with the doubling occurring every 18 months rather than two years. That said, Moore’s law is an observation of the semiconductor industry. Although it is very tempting to hope, it is unlikely to be just a matter of time before we are able to download a 1 GByte operating system upgrade in 25 seconds at 326.4 Mbps from a cellular system to our laptop while riding an elevator on the way to a meeting.
Probing the Shannon-Hartley Theorem
Techniques such as interference cancellation (IC) and spatial diversity with multi-stream transmission appear to get around the theorem but looking a bit closer this is not strictly true. The potential of IC in cellular systems is due to most noise not being truly Gaussian as assumed by the theorem. If information can be extracted from this “noise” then it is “others’ signal” and can be removed, thereby improving capacity. The challenge is in the processing power and advanced algorithms required to track, decode and then remove the dynamic interference from multiple users. This puts a practical and modest upper limit on what can be achieved. For spatial diversity, the theorem still indicates the capacity of each channel and it is the correlation between the channels that would determine the overall improvement possible using multiple-input/multiple-output (MIMO) techniques.
Pinpointing the Origins of Higher Data Rates
If we take a closer look at the evolution of data rates and spectral efficiency for each system, we discover six technical factors that explain the growth:
Accounting for Interference
Unlike wired communication channels such as copper or fiber which largely isolate signals from each other, electromagnetic propagation in free space knows no boundaries. On first inspection, the Shannon-Hartley theorem predicts that for LTE to deliver
100 Mbps in a single channel would require an SNR of better than 30 dB. This is a crucial point: In a typical environment, how often does the SNR reach such levels?
In the limit case of an isolated cell (e.g., a hotspot), demonstrating peak performance is straightforward and only limited at the cell boundaries when the self-noise of the system becomes dominant. However, when the cells become closer to the point where coverage is continuous, the interference situation is very different.
Examining the Distribution of Geometry Factor
Figure 3 shows the distribution of G factor that would be typical for randomly distributed outdoor users in a major metropolitan area. Of note, 20 percent of users experience a G factor below 0 dB, the 50 percentile point is at 5 dB, and only 10 percent of users experience better than 15 dB. For indoor — particularly at frequencies well above 1 GHz where building penetration loss is significant — conditions degrade and the distribution would move significantly to the left. This is a big concern for QoE given the high proportion of cellular calls that are made indoors. Dedicated indoor networks are the only realistic way round this
Comparing Wi-Fi and Femtocells for High Data Rates
Today we have significant deployment of private and public wireless access based on IEEE 802.11 (Wi-Fi). These have improved in performance and coverage at a remarkable rate. Unfortunately, though, their simpler technologies and unlicensed operating band are very prone to interference and have become a victim of their own success in some areas. The lack of transmit power control considered essential for cellular is a major issue. Fortunately, with over 600 MHz of spectrum at 2.4 and 5 GHz, Wi-Fi has more room to expand and thus fewer efficiency worries than cellular. An alternative to Wi-Fi is the emerging cellular “home base station” or femtocell. These have been proposed and even standardized but have never taken off.3 Now, there is evidence that the situation may be changing. The two big challenges for femtocells are cost versus Wi-Fi and interference mitigation to protect the licensed cellular network.
Looking to the Future
The physical and commercial constraints on implementing high-data-rate cellular services must be considered. As with transportation systems where there is a wide mix of vehicle types to match the range of channels, so it will be with wireless. The cellular industry needs to continue to optimize performance for the average user as defined by the statistics of the radio channel and not risk getting distracted by peak performance. Cellular’s focus should move from technology towards the development of compelling services with high QoE. The battle for the high-data-rate home and enterprise wireless markets will continue, and whether the winner is based on Wi-Fi or the more advanced femtocells, Keysight Technologis, Inc. is ready to provide the tools the industry needs to design and optimize the right wireless technology for the future.
×
*Indicates required field
Thank you.
A sales representative will contact you soon.