What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
5DX Automated X-ray Inspection Edgeport Driver Version 3.60
Symptom: Replacement Edgeport USB to RS-232 communications converter box is incompatible, preventing reliable RS-232 communications.
Problem Description: Edgeport USB to RS-232 converter has a changed internal "Chip-set" causing incompatibility problems for the 5DX IPC computer.
Solution: Install attached Edgeport Driver version 3.60 when replacing Edgeport Box and when performing a 5DX System Controller recovery.
Installation Procedure:
- Download and unzip the Edgeport Driver 3.60 file below to a temporary folder on 5DX System Controller.
- Go to Control Panel.
- Select System.
- Select Hardware Tab.
- Select Device Manager button.
- Select Multi-port serial adapters
- Select Inside-Out Network Edgeport/4
- Select Driver tab
- Select Update Driver button.
- Select “Yes, this time only”. Click next.
- Select “Install from a list or specific location”. Click next.
- Select “Search for the best driver in these locations”.
- Only check box “Include this location in the search”.
- Enter temporary folder location from step 1 and click next.
- After installation the IonMultiPortSerial icon will appear in the Device Manager window.
- Restart computer.
- Go to Start menu → All Programs → Inside Out Networks → Edgeport Configuration Utility.
- Click on Configure, manually change the Port numbers:
- Port 1 = 3
- Port 2 = 4
- Port 3 = 5
- Port 4 = 6
Note: Edgeport Driver version 3.60 will work with the changed “Chip-set” and the older “Chip-set”.
Please direct questions or comments to: emt-hstd-support_americas@keysight.com
Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum | Version | Versionsbeschreibung |
---|---|---|
2007-01-10 | 3.60 | N/A |
Veröffentlichungsdatum | Version |
---|---|
2007-01-10 | 3.60 |
Version Description |
---|
N/A |
How to Download
- See Above
How to Install
- See Above
Lizenzierung
- Requires a License
Keine Softwareversion verfügbar
SHOW MORE