Overview
The standard definition file of the 85038A/F/M(7-16 Calibration kits) can be imported into the ENA by following procedure.

[E5070B/71B firmware revision A.05.02 or below]
Can not use 85038A/F/M. Please update firmware.

[E5070B/71B firmware revision A.06.00 thru A.06.51]
Please update firmware. If you still want to use these firmware revision, definition file of 85038A/F/M can be loaded to ENA by following procedure.
Step1. Right click the "85038.CKX" listed below then select "save target as...", then save file to the floppy disk.
Step2. Copy the "85038.CKX" to the D drive of the ENA.
Step3. Import the definition file by "Calibration" > "Modify Cal Kit" > "Import cal kit".

[E5070B/71B firmware revision A.08.01 or later]
On the installation of the new firmware, 85038A/F/M is automatically loaded as the 10th of pre-defined cal kit.
However, if the 10th cal kit of ENA is already defined by user, 85038A/F/M will not be overwritten. Please activate 85038A/F/M by following procedure.
Step1. [Cal] > "cal kit" > Select 10th cal kit
Step2. [Cal] > "Modify cal kit" > "Restore Cal Kit" > "OK"

[E5071C firmware revision A.07.01 or A.07.02]
Please update firmware. If you still want to use these firmware revision, definition file of 85038A/F/M can be loaded to ENA by following procedure.
Step1. Right click the "85038.CKX" listed below then select "save target as...", then save file to the USB memory.
Step2. Copy the "85038.CKX" to the D drive of the ENA.
Step3. Import the definition file by "Calibration" > "Modify Cal Kit" > "Import cal kit".

[E5071C firmware revision A.08.01 or later]
On the installation of the new firmware, 85038A/F/M is automatically loaded as the 10th of pre-defined cal kit.
However, if the 10th cal kit of ENA is already defined by user, 85038A/F/M will not be overwritten. Please activate 85038A/F/M by following procedure.
Step1. [Cal] > "cal kit" > Select 10th cal kit
Step2. [Cal] > "Modify cal kit" > "Restore Cal Kit" > "OK"

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2006-01-11 n/a The calibration definition file of the 85038A/F/M for the ENA
Release Date Version
2006-01-11 n/a
Version Description
The calibration definition file of the 85038A/F/M for the ENA

How to Download

  • See Above

How to Install

  • See Above

Licensing

  • Does Not Require a License

Installs on: Instrument

Operating System

  • Windows XP

Prerequisites

  • See Above

Supported Instruments

  • E5070A, E5071A, E5070B, E5071B, E5071C, E5061A, E5062A
No previous versions available
SHOW MORE