This printer driver is only used for the E5071A with the following serial numbers and for using the HP DeskJet 940C with the E5071A. This driver is not required if the software has already been installed into the E5071A.

E5071A JP1KJ00100 through 248,251,253.

Required E5071A Firmware Revision

Rev.A.01.00 and above

Installation Procedure

Step1. Prepare five floppy disks.
Step2. Label disk with disk number (e.g. disk1, disk2, .. disk5).
Step3. Insert the floppy disk labeled "disk1" into your computer's FDD.
Step3. Click on the "Printer driver [disk1]" listed below.
Step4. Copy the file onto the disk.
Step5. Repeat each file onto each disk.

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2002-08-19 n/a Printer driver [disk1]
Release Date Version
2002-08-19 n/a
Version Description
Printer driver [disk1]

How to Download

  • Download all of files.

How to Install

  • See Above

Licensing

  • Does Not Require a License

Add-On Software / Utilities

Installs on: PC

Operating System

  • Windows XP

Prerequisites

  • See Above

Supported Instruments

  • E5070A E5071A
No previous versions available
SHOW MORE