What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
Baseband Studio Installation Software
Note: The Keysight IO Libraries installation program will generate an "IKernel.exe Application Error" at the end of the installation process. The Application Error dialog box will display a message similar to the following: 'The instruction at "0x771c741a" referenced memory at "0x00164780". The memory could not be "read"'. This error can safely be ignored since it occurs after the IO Libraries have been successfully installed. For more information about using Keysight IO Libraries with Windows XP, please refer to the "IO Libraries Readme" file in the Keysight IO Libraries program folder that you can access from the Microsoft Windows Start menu after installation.
キーサイトは、最新のバグ修正とセキュリティパッチを含む、利用可能な最新バージョンを使用することをお勧めします。
リリース | バージョン | 内容 |
---|---|---|
2004-11-05 | 1.2.1 | Includes: Baseband Studio Platform 1.1.2; fading software 1.2.2; streaming software 1.1.10; Windows 2000 PCI card driver 2.0.4; Keysight IO Libraries M.01.01.02; Baseband Studio Platform Help 1.1.0; Microsoft .NET Framework 1.0.3705. |
リリース | バージョン |
---|---|
2004-11-05 | 1.2.1 |
Version Description |
---|
Includes: Baseband Studio Platform 1.1.2; fading software 1.2.2; streaming software 1.1.10; Windows 2000 PCI card driver 2.0.4; Keysight IO Libraries M.01.01.02; Baseband Studio Platform Help 1.1.0; Microsoft .NET Framework 1.0.3705. |
ダウンロード方法
- Click the Download button
- Select the appropriate executable file
- Choose Run
インストール方法
- Select the appropriate executable file
- Choose Run
ライセンス
- Does Not Require a License
Installs on: PC
OS
- 2000 Service Pack 2
- 2000 Service Pack 3
- XP Service Pack1
前提知識
None
対象測定器
- N5110A, N5115A, N5115B
ダウンロード方法
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
インストール方法
- Select the appropriate executable file.
- Choose Run.
ライセンス
- Does Not Require a License
Installs on: PC
OS
- 2000 Service Pack 2
- 2000 Service Pack 3
- XP Service Pack 1
前提知識
None
対象測定器
- N5110A, N5115A, N5115B
ダウンロード方法
- Click the Download button
- Select the appropriate executable file
- Choose Run
インストール方法
- Select the appropriate executable file
- Choose Run
ライセンス
- Does Not Require a License
Installs on: PC
OS
- 2000 Service Pack 2
- 2000 Service Pack 3
- XP Service Pack 1
前提知識
None
対象測定器
- N5110A, N5115A, N5115B
SHOW MORE