What are you looking for?
KS8109A Resource Arbiter Client
Verification of devices, especially production, usually involves a set of test procedures using multiple instruments. To achieve high throughput and minimize cost of test it is necessary to make best use of the instruments and other resources by performing procedure steps in parallel and sharing instruments when testing multiple devices.
A typical software configuration includes the KS8108A Resource Arbiter Server license, one or more KS8109A Resource Arbiter Client licenses together with KS8000A or KS8400A Pathwave Test Automation licenses, and optionally the plugins for instruments and other resources.
發佈日期 | 版本 | 版本說明 |
---|---|---|
2021-06-22 | 1.2.4 | Miscellaneous fixes |
發佈日期 | 版本 |
---|---|
2021-06-22 | 1.2.4 |
Version Description |
---|
Miscellaneous fixes |
如何下載
- Click the Continue button.
- Save the TapPackages file to your PC.
如何安裝
Perform ANY of the following steps:
- Using the CLI from your PathWave Test Automation installation directory, type:
tap package install "package_file"
-
If the Developer's System is installed and simply double-clicking the downloaded package file does not work for this TapPackages file, download the following Resource Arbiter packages from the OpenTAP Package repository (http://packages.opentap.io) and install simply via double clicking the TapPackage files in the following order:
- Resource Placeholders TapPackage
- Resource Arbiter Shared TapPackage
- Resource Arbiter Client TapPackage
授權
- Requires a License
支援文件
如何下載
- Click the Continue button.
- Save the TapPackages file to your PC.
如何安裝
Perform ANY of the following steps:
- Using the CLI from your PathWave Test Automation installation directory, type:
tap package install "package_file"
-
If the Developer's System is installed and simply double-clicking the downloaded package file does not work for this TapPackages file, download the following Resource Arbiter packages from the OpenTAP Package repository (http://packages.opentap.io) and install simply via double clicking the TapPackage files in the following order:
- Resource Placeholders TapPackage
- Resource Arbiter Shared TapPackage
- Resource Arbiter Client TapPackage
授權
- Requires a License
支援文件
- Lock and Allocate instruments
- Easy switch integration and routing using OpenTAP or PathWave Test Automation
- REST API for use from any Client
如何下載
Click the Continue button Save or run the TapPackage
如何安裝
Double-click the .TapPacakge file or
Install directly from the OpenTAP Package repo (http://packages.opentap.io) using the PathWave Test Automation Package Manager.
授權
- Requires a License