Verification of devices, especially production, usually involves a set of test procedures using multiple instruments. To achieve high throughput and minimize cost of test it is necessary to make best use of the instruments and other resources by performing procedure steps in parallel and sharing instruments when testing multiple devices.

A typical software configuration includes the KS8108A Resource Arbiter Server license, one or more KS8109A Resource Arbiter Client licenses together with KS8000A or KS8400A Pathwave Test Automation licenses, and optionally the plugins for instruments and other resources.
 

是德建議使用最新的版本,其中包括最新的漏洞修復與安全覆蓋
免費 Trial
發佈日期 版本 版本說明
2021-06-22 1.2.4 Miscellaneous fixes
發佈日期 版本
2021-06-22 1.2.4
Version Description
Miscellaneous fixes

如何下載

  1. Click the Continue button.
  2. Save the TapPackages file to your PC.

如何安裝

  • Perform ANY of the following steps:

    • Using the CLI from your PathWave Test Automation installation directory, type:

    tap package install "package_file"

  • If the Developer's System is installed and simply double-clicking the downloaded package file does not work for this TapPackages file, download the following Resource Arbiter packages from the OpenTAP Package repository (http://packages.opentap.io) and install simply via double clicking the TapPackage files in the following order:
    • Resource Placeholders TapPackage
    • Resource Arbiter Shared TapPackage
    • Resource Arbiter Client TapPackage

授權

  • Requires a License

Installs on: PC

作業系統

  • Windows 10

如何下載

  1. Click the Continue button.
  2. Save the TapPackages file to your PC.

如何安裝

  • Perform ANY of the following steps:

    • Using the CLI from your PathWave Test Automation installation directory, type:

    tap package install "package_file"

  • If the Developer's System is installed and simply double-clicking the downloaded package file does not work for this TapPackages file, download the following Resource Arbiter packages from the OpenTAP Package repository (http://packages.opentap.io) and install simply via double clicking the TapPackage files in the following order:
    • Resource Placeholders TapPackage
    • Resource Arbiter Shared TapPackage
    • Resource Arbiter Client TapPackage

授權

  • Requires a License

Installs on: PC

作業系統

  • Windows 10
  • Lock and Allocate instruments
  • Easy switch integration and routing using OpenTAP or PathWave Test Automation
  • REST API for use from any Client

如何下載

  • Click the Continue button Save or run the TapPackage

如何安裝

  • Double-click the .TapPacakge file or

  • Install directly from the OpenTAP Package repo (http://packages.opentap.io) using the PathWave Test Automation Package Manager.
     

授權

  • Requires a License

Installs on: PC

作業系統

  • Windows 10
SHOW MORE