Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2018-06-29 A.2 U1831C firmware version A.2
Veröffentlichungsdatum Version
2018-06-29 A.2
Version Description
U1831C firmware version A.2

How to Download

  • Click on the "Download" button.
  • Save the firmware.zip file to your computer and note the directory where the file is saved.
  • Unzip the file, ensure the 4 files are available (WinUSB Driver folder, A.2_Upgrade.hex, HID_Bootloader_PIC18_Integrated and mcHID.dll).
  • NOTE: The .net framework 3.5 is required to upgrade U1831C firmware.

How to Install

  1. Connect DUT to PC.
  2. Install "WinUSB Driver" to the PC. To do so, right-click on "My Computer/This PC" and select "Properties". Click on "Device Manager". Select the DUT connected (under "Universal Serial Bus Controller") and expand the list. Then right-click on the "U183XX External USB Smart Noise Source" and subsequently "Update Driver Software". Browse for the "WinUSB Driver" folder and proceed for installation.
  3. Save "mcHID.dll" into C:\Windows\system folder.
  4. Click on the "HID_Bootloader_PIC18_Integrated.exe" file. The firmware upgrade window will appear.
  5. Select the DUT to be upgraded from the list. Click on the "Upgrade" button.
  6. Click on "Open Hex File" to select the "A.2_Upgrade.hex" downloaded earlier.
  7. Click on "Program/Verify" button. Once completed a message "Program/Verify Passed" will appear.
  8. Click on the "Reset Device" button. The DUT is now ready with the new firmware installed.

Lizenzierung

  • Does Not Require a License

Installs on: PC / Instrument

Operating System

  • Windows 7
  • Windows XP
  • Windows 10

Voraussetzungen

  • Information Not Available

Supported Instruments

  • U1831C
Keine Softwareversion verfügbar
SHOW MORE