What are you looking for?
KS8106A REST API Plugin Software
Download and install the latest KS8106A REST API Plugin software.
发布日期 | 版本 | 版本说明 |
---|---|---|
2020-09-15 | 2.0.0 | Initial 2.x release 2.0.0+fd62a702 |
发布日期 | 版本 |
---|---|
2020-09-15 | 2.0.0 |
Version Description |
---|
Initial 2.x release 2.0.0+fd62a702 |
What's new in version 2.0?
- We provide supported client libraries for C# and TypeScript.
- Added support for OpenAPI to allow generating clients for other programming languages.
- Switch to use the new OpenTAP Annotation system to alleviate differences in property editing between the OpenTAP Editor and the REST-API.
- Simplification of advanced endpoints.
What changed in version 2.0?
- Using the REST-API Plugin is now significantly simpler. Previously, lots of boilerplate code was needed to deal with endpoints and parsing JSON responses. In version 2.0, with the help of OpenAPI, that is all abstracted into a user friendly and strongly typed client library. To support this, all endpoints and their JSON content have changed; however, concepts remain the same.
- "Proxy mode" has been renamed to "SessionManager mode" and the proxy/redirect functionality of Session endpoints through the Proxy/SessionManager has been removed.
如何下载
- Click the Continue button
- Save or run the Installer
Can also be downoload from the OpenTAP Package Repo: http://packages.opentap.io/index.html#/ name=REST-API
如何安装
- Double-click on the downloaded .tappackage to run the installer
or
From a Command Line:
cd %TAP_PATH%
tap package install "REST API" -r https://packages.opentap.io
颁发许可证
- Requires a License
Various bug fixes and performance improvements
如何下载
- Click the Continue button
- Save or run the installer
如何安装
Double Click on downloaded TAP Package to the the installer
or
from a command line run:
tap package install "REST API" -r https://packages.opentap.io
颁发许可证
- Requires a License
- Various performance improvements and bug fixes
-
View installed REST-API-Documentation.pdf for complete changelog
如何下载
- Click the Download button.
- Save or run the installer.
如何安装
- Double-click on downloaded software file to run the installer.
颁发许可证
- Requires a License
Extended API and updated to work with OpenTAP
View installed REST-API-Documentation.pdf for complete changelog
如何下载
- Click the Download button.
- Save or run the installer.
如何安装
- Double-click on downloaded software file to run the installer.
颁发许可证
- Requires a License
The KS8106A REST-API allows for web-based control and/or integration with TAP both locally or remotely.
如何下载
- Click the Download button.
- Save or run the installer.
如何安装
- Double-click on downloaded software file to run the installer.
颁发许可证
- Requires a License
KS8106A REST API Plugin software download for Windows.
如何下载
- Click the Download button.
- Save or run the installer.
如何安装
- Double-click on downloaded software file to run the installer.
颁发许可证
- Requires a License