Situation:

After April 18th 2018, i1000 software will report a “VTEP License Not found” error during start-up, VTEP learning or VTEP diagnostics, even though the license file is valid.

The i1000 software, including the VTEP software will continue to function in production, however VTEP learning, debugging and diagnostics functionalities will not work any more.

This issue happens across all i1000D system types and all versions of the software.

Solution/Action:

A software issue has been identified and a software patch has been created and is available for download.

After downloading, the “VTEP_Fix_setup.exe” can be run directly and after restarting i1000 software, the error message will not show up and VTEP should be working as it is desired.
 

キーサイトは、最新のバグ修正とセキュリティパッチを含む、利用可能な最新バージョンを使用することをお勧めします。
リリース バージョン 内容
2018-04-27 NA Hot fix to resolve VTEP error
リリース バージョン
2018-04-27 NA
Version Description
Hot fix to resolve VTEP error

ダウンロード方法

  • Click the "Download" button.
    Save file to a folder in C: drive of PC.

インストール方法

  • Double click on the downloaded file.

ライセンス

  • Does Not Require a License

Installs on: PC

OS

  • Windows 7

前提知識

  • No prerequisite required.

ソフトウェアバージョンはご利用いただけません
SHOW MORE