What are you looking for?
BT2152A/B Self-Discharge Analyzer Firmware
BT2152A/B Self-Discharge Analyzer Firmware
Data de lançamento | Versão | Descrição da Versão |
---|---|---|
2023-10-24 | A.04.79 | Adds support for Rev. 6 of P600 module, operation up to 4.5V, and temperature measurement down to -20 deg. C |
Data de lançamento | Versão |
---|---|
2023-10-24 | A.04.79 |
Version Description |
---|
Adds support for Rev. 6 of P600 module, operation up to 4.5V, and temperature measurement down to -20 deg. C |
BT2152A/B Self-Discharge Analyzer Firmware
Como Baixar
- Click the Download button.
- Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
- Unzip the file to access the .upd file.
Como Instalar
From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
Licenciamento
- Does Not Require a License
Documentação de suporte
Software / Utilitários Complementares
Installs on: Instrument
Sistema Operacional
- Windows 7
- Windows XP
- Windows 10
Pré-requisitos
- Information Not Available
Instrumentos Compatíveis
- BT2152A, BT2152B
BT2152A/B Self-Discharge Analyzer Firmware
Como Baixar
- Click the Download button.
- Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
- Unzip the file to access the .upd file.
Como Instalar
From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
Licenciamento
- Does Not Require a License
Documentação de suporte
Software / Utilitários Complementares
Installs on: Instrument
Sistema Operacional
- Windows 7
- Windows XP
- Windows 10
Pré-requisitos
- Information Not Available
Instrumentos Compatíveis
- BT2152A, BT2152B
Como Baixar
- Click the Download button.
- Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
- Unzip the file to access the .upd file.
Como Instalar
From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
Licenciamento
- Does Not Require a License
Documentação de suporte
Software / Utilitários Complementares
Installs on: Instrument
Sistema Operacional
- Windows 7
- Windows XP
- Windows 10
Pré-requisitos
- Information Not Available
Instrumentos Compatíveis
- BT2152A
Como Baixar
- Click the Download button.
- Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
- Unzip the file to access the .upd file.
Como Instalar
From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
Licenciamento
- Does Not Require a License
Documentação de suporte
Software / Utilitários Complementares
Installs on: Instrument
Sistema Operacional
- Windows 7
- Windows XP
- Windows 10
Pré-requisitos
- Information Not Available
Instrumentos Compatíveis
- BT2152A
Como Baixar
- Click the Download button.
- Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
- Unzip the file to access the .upd file.
Como Instalar
From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
Licenciamento
- Does Not Require a License
Documentação de suporte
Software / Utilitários Complementares
Installs on: Instrument
Sistema Operacional
- Windows 7
- Windows XP
- Windows 10
Pré-requisitos
- Information Not Available
Instrumentos Compatíveis
- BT2152A
Como Baixar
- Click the Download button.
- Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
- Unzip the file to access the .upd file.
Como Instalar
From the utility directory or Start menu, start the utility FWUpdate.exe (a link to this utility can be found directly below). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility. It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
Licenciamento
- Does Not Require a License
Documentação de suporte
Software / Utilitários Complementares
Installs on: Instrument
Sistema Operacional
- Windows 7
- Windows XP
- Windows 10
Pré-requisitos
- Information Not Available
Instrumentos Compatíveis
- BT2152A