是德建议使用最新的版本,其中包括最新的漏洞修复和安全补丁
发布日期 版本 版本说明
2015-12-09 01.00.0003 The N7015A/N7016A USB Type-C Interconnect Assembly Controller software is used to configure the hardware settings of the low speed fixture.
发布日期 版本
2015-12-09 01.00.0003
Version Description
The N7015A/N7016A USB Type-C Interconnect Assembly Controller software is used to configure the hardware settings of the low speed fixture.

如何下载

  • Click the download button and save the file to a temporary directory on your Infiniium oscilloscope or personal computer.

如何安装

  • The N7015A/N7016A USB Type-C Interconnect Assembly Controller software should be installed on the Infiniium oscilloscope or personal computer that will be used to configure the hardware settings of the N7016A low speed fixture.

  • To install the software, open (execute) the downloaded file, and follow the on-screen installation instructions.

颁发许可证

  • Does Not Require a License

Installs on: PC / Instrument

操作系统

  • Windows 7
  • Windows Vista

前提要求

  • Microsoft .NET 4.5.2 software

支持的仪器

  • N7016A Low Speed Fixture
没有可用的软件版本
SHOW MORE