What are you looking for?
VISA Shared Components downloads
The VISA Shared Components is a required component for the IO Libraries Suite to operate correctly. The correct version of the VISA Shared Components is installed by the IO Libraries Suite, so users don't typically need to worry about installing this package.
However, if you need to repair, or install an older version of the VISA Shared Components you can download it here.
Veröffentlichungsdatum | Version | Versionsbeschreibung |
---|---|---|
2013-12-01 | 1.6 | Updated the USB-TMC kernel driver to address issues with USB 3.0. Added support for the new VISA COM interface IRegister64_2. Changed the downloadable installer to be a self-extracting EXE rather than the raw MSI. |
Veröffentlichungsdatum | Version |
---|---|
2013-12-01 | 1.6 |
Version Description |
---|
Updated the USB-TMC kernel driver to address issues with USB 3.0. Added support for the new VISA COM interface IRegister64_2. Changed the downloadable installer to be a self-extracting EXE rather than the raw MSI. |
How to Download
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
How to Install
Run the downloaded installer
Lizenzierung
- Does Not Require a License
Supporting Documentation
Add-On Software / Utilities
Installs on: PC
Operating System
- Windows 8
- Windows 7
- Windows Vista
- Windows XP
Voraussetzungen
No prerequisites.
How to Download
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
How to Install
Run the downloaded installer
Lizenzierung
- Does Not Require a License
Supporting Documentation
Add-On Software / Utilities
Installs on: PC
Operating System
- Windows 8
- Windows 7
- Windows Vista
- Windows XP
Voraussetzungen
No prerequisites.
The header file visatype.h was not being installed into "Win64\Include" subdirectory. The header file visa.h was missing the definition for VI_INTF_USB. A device that claimed to be compliant with USB-TMC but had an incorrect interrupt pipe configuration could cause ausbtmc.sys to blue-screen. Various fixes to viWaitOnEvent in Win64 shared version of visa64.dll. The VISA COM interfaces IRegister64, ISharedRegister64, IHislipInstr and IPxi were not being properly registered. Updated binaries from Visual Studio 2005 to 2008 and changed the runtime version that is included in the installer.
How to Download
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
How to Install
Run the downloaded installer
Lizenzierung
- Does Not Require a License
Supporting Documentation
Add-On Software / Utilities
Installs on: PC
Operating System
- Windows 8
- Windows 7
- Windows Vista
- Windows XP
Voraussetzungen
No prerequisites.
How to Download
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
How to Install
Run the downloaded installer
Lizenzierung
- Does Not Require a License
Supporting Documentation
Add-On Software / Utilities
Installs on: PC
Operating System
- Windows 7
- Windows Vista
- Windows XP
Voraussetzungen
No prerequisites.