For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

Keysight는 가능한 최신 버전을 사용하는 것을 권장하며, 최신 버전에는 현재 사용 가능한 가장 최신 버그 수정 및 보안 패치가 포함되어 있습니다.
릴리스 날짜 버젼 버전 설명
2020-06-22 2.1.1006.3 Windows 10 support
릴리스 날짜 버젼
2020-06-22 2.1.1006.3
Version Description
Windows 10 support

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description:

  • Added support for detector type Peak.
  • Further enhanced 89600 VSA control with M9203A 1 GHz module.
  • New M9214A IF Digitizer FPGA bits to fix issues with dither setup being ignored with board rev numbers greater than 2.

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7
  • Windows 10

지원되는 계측기

  • M9393A (modules supported: M9214A, M9308A, M9365A, M9169E)

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description:

  • Added support for detector type Peak.
  • Further enhanced 89600 VSA control with M9203A 1 GHz module.
  • New M9214A IF Digitizer FPGA bits to fix issues with dither setup being ignored with board rev numbers greater than 2.

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 8
  • Windows 7

지원되는 계측기

  • M9393A (modules supported: M9214A, M9308A, M9365A, M9169E)

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description:

  • When the M9393A driver is initialized with “ExternalDigitizer=true” or “ExternalDigitizer=1” in the option string, M9214A IF Digitizer is no longer required in the PXI chassis.
  • A new M9393 wideband IF hardware extension for the 89600 VSA has been added that allows a M9393A to be paired with a M9203A digitizer to obtain measurement bandwidth up to 1 GHz.
  • New FPGA bits with improved stability.

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 8
  • Windows 7

지원되는 계측기

  • M9393A (modules supported: M9214A, M9308A, M9365A, M9169E)

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description:

  • Enhanced support for list mode with external attenuator configuration.
  • Corrected external attenuator module identification.
  • Corrected selection of external attenuator module in simulation mode.
  • Corrected field alignment backwards compatibility with 1.x factory calibration data.
  • Corrected resource locking for the M9300 Reference module.

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 8
  • Windows 7

선결 조건

지원되는 계측기

  • M9393A (modules supported: M9214A, M9308A, M9365A, M9169E)

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description :

  • Added property, RF3.Attenuator, to select RF attenuator type used for certain hardware configurations.
  • Added property, RF3.AttenuatorMode, to control the RF input signal path in front of the mixer.
  • Added interface, FFTAcquisition2.NoiseCorrection, with properties Enabled and Mode to support noise correction in FFT acquisition mode.
  • M9300A-Carrier FPGA 1.0.4.0 available – Optional, not currently required for any new software features.

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 8
  • Windows 7

선결 조건

지원되는 계측기

  • M9393A (modules supported: M9214A, M9308A, M9365A, M9169E)

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description :

  • Enhanced self-tests and corrections for installed hardware options.
  • Enhanced support for external applications software.
  • Increased IF frequency range to [200 MHz, 800 MHz] for external wideband digitizers.

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 8
  • Windows 7

지원되는 계측기

  • M9214A, M9300A, M9308A, M9365A, M9169E

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version Description :

  • Support for extended frequency range (3.6 GHz - 50 GHz) using option M9365A-FRX. Use of M9169E Programmable Attenuator is recommended for range control, automated field alignments, and self test.
  • Support for wideband IF (up to 800 MHz) using option M9365A-WB1 and use of an external wideband digitizer, such as M9202A or M9703A.
  • Limited (setup) support for data streaming using the M9202A wideband digitizer. All streaming controls are available from the M9392A VSA Soft Front Panel and IVI interfaces.
  • Support for peer-to-peer IQ data transfer from the M9214A Digitizer module to another module that supports peer-to-peer data transfer, such as the M9451A module, using the PeertoPeerPort IVI interface.
  • Enhanced self-tests for extended frequency ranges with or without the M9169E Step Attenuator.
  • 89600: Power Spectrum speed improvements

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 8
  • Windows 7

선결 조건

지원되는 계측기

  • M9214A, M9300A, M9308A, M9365A, M9169E

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version Description :

Various defects fixed:

  • Corrected frequency scaling for soft front panel FFT Acquisition mode
  • Increased maximum value for soft front panel IQ averaging period to match IVI maximum
  • Fixed intermittent glitch on narrowband time trace after using FFT Acquisition mode

     

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7

지원되는 계측기

  • M9214A, M9300A, M9308A, M9365A

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version Description :

Added Support for M9415A Peer To Peer operation. Not supported via IVI.
Added Support for M9415A Noise Correction in FFT Acquisition Mode. Not supported via IVI.
 

Various defects fixed:
WIT 385288 – LO Feedthrough causes IF Overloads when using Noise Corrections
WIT 391319 – Interaction with M90XA prevents newer M90XA versions from running

 

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7

선결 조건

지원되는 계측기

  • M9214A, M9300A, M9308A, M9365A

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP

선결 조건

지원되는 계측기

  • M9214A, M9300A, M9308A, M9365A

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version description:

  • 89600: allow driver sharing using M9000 resource manager for multi-channel configurations
  • Various defects fixed:
    • WIT 353338 – Issue starting system if locale uses comma as decimal separator
    • WIT 357918 – LO Nulling intermittently fails on some systems
    • WIT 369709 – Issue with field calibration resulting in ~0.2 dB flatness error on some units
    • WIT 335725 – 89600: error reported when IF Dither enabled and Span/RBW ratio too large
    • WIT 353408 – 89600: error reported when switching between IF Mag & External Trigger in Sequenced Mode
    • WIT 353905 – 89600: minimum gate length limited to 100 ns in zero span
    • WIT 355118 – 89600: added VBW limiting in zero span
    • WIT 356920 – 89600: channel filter was not set correctly for non-power spectrum measurements
    • WIT 359033 – 89600: allow higher Span to RBW ratio based on physical memory available 

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7

지원되는 계측기

  • M9393A, M9214A, M9300A, M9308A, M9365A

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.1.2

Version description:

  • Added LabVIEW driver for M9393A
  • Added IF Dither mode for Stepped Spectrum
    • See IAgM9393Ex2.SteppedSpectrumAcquisition2.IFDither.*
  • Added multi-channel synchronization
    • See IAgM9393.MultiChannelSync.*
  • Defect WIT 337258: 89600 - Overlap Percentage error with Gate Trigger and Power Spectrum
  • Defect WIT 339914: Comprehensive alignment failed if initial instrument state is Stepped Spectrum and conversion is image protect
  • Documentation updates
     

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7

지원되는 계측기

  • M9393A, M9214A, M9300A, M9308A, M9365A

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7

지원되는 계측기

  • M9393A, M9214A, M9300A, M9308A, M9365A

다운로드 방법

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

설치 방법

  • Run the downloaded installer.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Windows 7

지원되는 계측기

  • M9393A, M9214A, M9300A, M9308A, M9365A
SHOW MORE