An update may take up to 60 minutes to complete depending on the type of components requiring an update. During this time, instrument modules installed in the chassis are deactivated to the ATCA service state to reduce power consumption and are unavailable for applications. The chassis fan speed may change during the update as well. Following the update, cycle chassis power to complete the installation.

A Keysight recomenda usar a versão mais atual, que inclui as correções de bugs e arquivos de segurança mais atualizados disponíveis.
Data de lançamento Versão Descrição da Versão
2014-08-04 2.3.11 If you are using a remote PC that has an Intel Haswell based processor, then you will need to use this firmware update.
Data de lançamento Versão
2014-08-04 2.3.11
Version Description
If you are using a remote PC that has an Intel Haswell based processor, then you will need to use this firmware update.

Como Baixar

  1. Click Download button
  2. Save .zip file to host computer (c:/tmp)
  3. Unzip the package to your PC

Como Instalar

  1. To open the M9521A Chassis Soft Front Panel, from Windows click:
  2. Start > All Programs > Agilent > AXIe Chassis (M9521) > AXIeC SFP
  3. From the SFP, click Utilities > Update Firmware... and follow the instructions in the dialog boxes and the application help.

Licenciamento

  • Does Not Require a License

Installs on: Instrument

Sistema Operacional

  • Windows 7 (SP1)
  • Windows 8.1

Pré-requisitos

  • IO Libraries 16.3 or later

Instrumentos Compatíveis

  • M9514A

Como Baixar

  1. Click Download button
  2. Save .zip file to host computer (c:/tmp)
  3. Unzip the package to your PC

Como Instalar

  1. To open the M9521A Chassis Soft Front Panel, from Windows click:
  2. Start > All Programs > Agilent > AXIe Chassis (M9521) > AXIeC SFP
  3. From the SFP, click Utilities > Update Firmware... and follow the instructions in the dialog boxes and the application help.

Licenciamento

  • Does Not Require a License

Installs on: Instrument

Sistema Operacional

  • Windows 7 (SP1)
  • Windows 8.1

Pré-requisitos

  • IO Libraries 16.3 or later

Instrumentos Compatíveis

  • M9514A
SHOW MORE