B1500A/B1505A Utility : IC-CAP MDM File Converter for B1500A/B1505A/EasyEXPERT

是德建议使用最新的版本,其中包括最新的漏洞修复和安全补丁
发布日期 版本 版本说明
2014-01-14 A.01.03 A.01.03.2014.0108
发布日期 版本
2014-01-14 A.01.03
Version Description
A.01.03.2014.0108

MDM File Converter A.01.03

如何下载

  • Click the "Download" button.

如何安装

  • 1. Expand the contents of the downloaded file into a working folder as follows.
        a) Go to the folder where the downloaded file is saved and open the folder.
        b) Place the pointer on the downloaded file and click the mouse right button
            and select "Extract All...".
        NOTE: If any unzip tool is installed, the above may not work.
                  In this case, follow the instruction of the tool.
                  Below is an example for the tool "winzip".
                  - Firstly double-click the donloaded file, then click "unzip" in the
                    menu bar. Then specify the folder and click "unzip".
    2. Insert the Desktop EasyEXPERT software CD-ROM into the CD-ROM drive.
    3. Double click the index.html file in the CD-ROM.
    4. Click "Install MDM File Converter" icon and follow the instructions of the setup wizard.
    5. Wait for installation to complete, and remove the CD-ROM from the CD-ROM drive.
     

颁发许可证

  • Does Not Require a License

支持文档

Installs on: PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

前提要求

  • See Readme file.

支持的仪器

  • B1500A, B1505A

MDM File Converter

如何下载

  • Click the "Download" button.

如何安装

  • 1. Expand the contents of the downloaded file into a working folder as follows.
        a) Go to the folder where the downloaded file is saved and open the folder.
        b) Place the pointer on the downloaded file and click the mouse right button
            and select "Extract All...".
        NOTE:  If any unzip tool is installed, the above may not work.
                   In this case, follow the instruction of the tool.
                   Below is an example for the tool "winzip".
                   - Firstly double-click the donloaded file, then click "unzip" in the
                     menu bar. Then specify the folder and click "unzip".
    2. Insert the Desktop EasyEXPERT software CD-ROM into the CD-ROM drive.
    3. Double click the index.html file in the CD-ROM.
    4. Click "Install MDM File Converter" icon and follow the instructions of the setup wizard.
    5. Wait for installation to complete, and remove the CD-ROM from the CD-ROM drive.
     

颁发许可证

  • Does Not Require a License

支持文档

Installs on: PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

前提要求

  • See Readme file.

支持的仪器

  • B1500A, B1505A
SHOW MORE