What are you looking for?
B1500A/B1505A Utility : IC-CAP MDM File Converter for B1500A/B1505A EasyEXPERT
B1500A/B1505A Utility : IC-CAP MDM File Converter for B1500A/B1505A/EasyEXPERT
Data de lançamento | Versão | Descrição da Versão |
---|---|---|
2014-01-14 | A.01.03 | A.01.03.2014.0108 |
Data de lançamento | Versão |
---|---|
2014-01-14 | A.01.03 |
Version Description |
---|
A.01.03.2014.0108 |
MDM File Converter A.01.03
Como Baixar
Click the "Download" button.
Como Instalar
1. Expand the contents of the downloaded file into a working folder as follows.
a) Go to the folder where the downloaded file is saved and open the folder.
b) Place the pointer on the downloaded file and click the mouse right button
and select "Extract All...".
NOTE: If any unzip tool is installed, the above may not work.
In this case, follow the instruction of the tool.
Below is an example for the tool "winzip".
- Firstly double-click the donloaded file, then click "unzip" in the
menu bar. Then specify the folder and click "unzip".
2. Insert the Desktop EasyEXPERT software CD-ROM into the CD-ROM drive.
3. Double click the index.html file in the CD-ROM.
4. Click "Install MDM File Converter" icon and follow the instructions of the setup wizard.
5. Wait for installation to complete, and remove the CD-ROM from the CD-ROM drive.
Licenciamento
- Does Not Require a License
Documentação de suporte
Installs on: PC
Sistema Operacional
- Windows 7
- Windows Vista
- Windows XP SP3
- Windows XP SP2
Pré-requisitos
See Readme file.
Instrumentos Compatíveis
- B1500A, B1505A
MDM File Converter
Como Baixar
Click the "Download" button.
Como Instalar
1. Expand the contents of the downloaded file into a working folder as follows.
a) Go to the folder where the downloaded file is saved and open the folder.
b) Place the pointer on the downloaded file and click the mouse right button
and select "Extract All...".
NOTE: If any unzip tool is installed, the above may not work.
In this case, follow the instruction of the tool.
Below is an example for the tool "winzip".
- Firstly double-click the donloaded file, then click "unzip" in the
menu bar. Then specify the folder and click "unzip".
2. Insert the Desktop EasyEXPERT software CD-ROM into the CD-ROM drive.
3. Double click the index.html file in the CD-ROM.
4. Click "Install MDM File Converter" icon and follow the instructions of the setup wizard.
5. Wait for installation to complete, and remove the CD-ROM from the CD-ROM drive.
Licenciamento
- Does Not Require a License
Documentação de suporte
Installs on: PC
Sistema Operacional
- Windows 7
- Windows Vista
- Windows XP SP3
- Windows XP SP2
Pré-requisitos
See Readme file.
Instrumentos Compatíveis
- B1500A, B1505A