B1500A/B1505A Utility : IC-CAP MDM File Converter for B1500A/B1505A/EasyEXPERT

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2014-01-14 A.01.03 A.01.03.2014.0108
Veröffentlichungsdatum Version
2014-01-14 A.01.03
Version Description
A.01.03.2014.0108

MDM File Converter A.01.03

How to Download

  • Click the "Download" button.

How to Install

  • 1. Expand the contents of the downloaded file into a working folder as follows.
        a) Go to the folder where the downloaded file is saved and open the folder.
        b) Place the pointer on the downloaded file and click the mouse right button
            and select "Extract All...".
        NOTE: If any unzip tool is installed, the above may not work.
                  In this case, follow the instruction of the tool.
                  Below is an example for the tool "winzip".
                  - Firstly double-click the donloaded file, then click "unzip" in the
                    menu bar. Then specify the folder and click "unzip".
    2. Insert the Desktop EasyEXPERT software CD-ROM into the CD-ROM drive.
    3. Double click the index.html file in the CD-ROM.
    4. Click "Install MDM File Converter" icon and follow the instructions of the setup wizard.
    5. Wait for installation to complete, and remove the CD-ROM from the CD-ROM drive.
     

Lizenzierung

  • Does Not Require a License

Supporting Documentation

Installs on: PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

Voraussetzungen

  • See Readme file.

Supported Instruments

  • B1500A, B1505A

MDM File Converter

How to Download

  • Click the "Download" button.

How to Install

  • 1. Expand the contents of the downloaded file into a working folder as follows.
        a) Go to the folder where the downloaded file is saved and open the folder.
        b) Place the pointer on the downloaded file and click the mouse right button
            and select "Extract All...".
        NOTE:  If any unzip tool is installed, the above may not work.
                   In this case, follow the instruction of the tool.
                   Below is an example for the tool "winzip".
                   - Firstly double-click the donloaded file, then click "unzip" in the
                     menu bar. Then specify the folder and click "unzip".
    2. Insert the Desktop EasyEXPERT software CD-ROM into the CD-ROM drive.
    3. Double click the index.html file in the CD-ROM.
    4. Click "Install MDM File Converter" icon and follow the instructions of the setup wizard.
    5. Wait for installation to complete, and remove the CD-ROM from the CD-ROM drive.
     

Lizenzierung

  • Does Not Require a License

Supporting Documentation

Installs on: PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

Voraussetzungen

  • See Readme file.

Supported Instruments

  • B1500A, B1505A
SHOW MORE