For a complete list of all IVI drivers from Keysight, please visit www.keysight.com/find/drivers

This driver download installs the IVI-C, IVI-COM, LabVIEW, and MATLAB driver components, as well as the soft front panel and kernel device driver.

Keysight modular drivers also require that Keysight IO Libraries Suite 16.0 or greater be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite

Current Version Details
Version 1.0.0.2
Models Supported M9168C
IO Libraries Required Version 16.0 or greater
Driver Types and Version IVI-C (32/64-bit) 1.0.6.0
IVI-COM (32/64-bit) 1.0.6.0
LabVIEW (32/64-bit) 1.0.2
MATLAB (32 bit) 1.0.6.0
Soft Front Panel Version 1.0.0.1
IVI Classes Supported IviDriver 1.0
Minimum IVI Shared Components Version 2.1.1


 

是德建议使用最新的版本,其中包括最新的漏洞修复和安全补丁
发布日期 版本 版本说明
2022-03-31 1.0.12.0 Fixed 64-bit issues
发布日期 版本
2022-03-31 1.0.12.0
版本说明
Fixed 64-bit issues

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

IVI driver version: 1.0.12.0

LabVIEW driver version: 1.1.4

如何下载

  1. Click the Download button. 
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run downloaded installer.

颁发许可证

  • Does Not Require a License

Installs on: PC

操作系统

  • Windows 7
  • Windows 10

支持的仪器

  • M9168C, M9168E, M9169E

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

IVI driver version: 1.0.9.0

LabVIEW driver version: 1.1.4

如何下载

  1. Click the Download button. 
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run downloaded installer.

颁发许可证

  • 不要求具有许可证

安装到: PC

操作系统

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP

支持的仪器

  • M9168C, M9168E, M9169E

如何下载

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run.

如何安装

  • See Readme File

颁发许可证

  • 不要求具有许可证

安装到: PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

前提要求

  • Keysight IO Libraries Suite
     

支持的仪器

  • M9168C, M9168E

如何下载

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run.

如何安装

  • See Readme File

颁发许可证

  • 不要求具有许可证

安装到: PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

支持的仪器

  • M9168C
SHOW MORE