您希望搜索哪方面的内容?
M950xA AXIe 机箱驱动程序
This driver download installs the IVI-C, IVI-COM, LabVIEW, and MATLAB driver components, as well as the soft front panel and kernel device driver.
Current Driver | Version 1.2.1.6 |
---|
For a complete list of all IVI drivers from Keysight, please visit www.keysight.com/find/drivers
Keysight modular drivers also require that Keysight IO Libraries Suite 16.0 or greater be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite
Version Details | ||
---|---|---|
Current Version | Previous Version | |
Version | 1.2.1.6 | 1.1.1 |
Models Supported | M9502A, M9505A | M9502A, M9505A |
IO Libraries Required Version | ≥ 1.6.2 |
≥ 16.0 Update 1 |
Driver Types and Version | IVI-C (32/64-bit) 1.2.1.6 IVI-COM (32/64-bit) 1.2.1.6 LabVIEW (32/64-bit) 1.2.1.6 MATLAB (32-bit) 1.2.1.6 |
IVI-C (32/64-bit) 1.1.1.1 IVI-COM (32/64-bit) 1.1.1.1 LabVIEW (32/64-bit) 1.1.1.1 MATLAB (32-bit) 1.1.1.1 |
Soft Front Panel Version | 1.2.1.6 | 1.1.1.1 |
IVI Classes Supported | 1.0 | IVIDriver 1.0 |
Minimum IVI Shared Components Version | 2.1.1 | 2.1.1 |
Version History | • Increased the chassis fan speed (requires chassis firmware version 1.3.23 or later). • Added support for Keysight IO Libraries 16.2. • On 64-bit systems, the Keysight IO Libraries version 16.2 32-bit mDNS responder patch is installed automatically. |
Initial Release |
发布日期 | 版本 | 版本说明 |
---|---|---|
2020-04-15 | 1.4.4.1 | See above. |
发布日期 | 版本 |
---|---|
2020-04-15 | 1.4.4.1 |
版本说明 |
---|
See above. |
Driver 1.4.4.1 fixes the issues below:
- Repair an enumeration and detection issue where the chassis cannot be detected in Keysight IO Libraries.
- This driver with combination of chassis firmware 1.3.44 together would repair an intermittent issue where the chassis is unable to communicate with modules after a boot up.
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), Labview (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0
如何下载
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
如何安装
- Run the downloaded installer.
颁发许可证
- 不要求具有许可证
驱动程序类型:IVI-C(32 位/64 位)、IVI-COM(32 位/64 位)、Labview(32 位/64 位)、MATLAB(仅限 32 位)
IVI 类型支持:IviDriver 1.0
如何下载
- 单击 “下载” 按钮。
- 选择适当的可执行文件。
- 选择 “运行”。
如何安装
- 运行下载的安装程序。
颁发许可证
- 不要求具有许可证
支持文档
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), Labview (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0
如何下载
-
Click the Download button.
-
Select the appropriate executable file.
- Choose Run.
如何安装
- Run the downloaded installer.
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 8
- Windows 7
- Windows XP
前提要求
IVI Shared Components 2.2.1.0 or later from www.ivifoundation.org
VISA Shared Components 1.6 or later from www.ivifoundation.org
支持的仪器
- M9502A, M9505A
相关链接
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)
IVI class support: IviDriver 1.0
如何下载
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
如何安装
Run the downloaded installer
颁发许可证
- 不要求具有许可证
支持文档
如何下载
1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run
如何安装
See Documentation
颁发许可证
- 不要求具有许可证