This driver download installs the IVI-C, IVI-COM, LabVIEW, and MATLAB driver components, as well as the soft front panel and kernel device driver.

Current Driver Version 1.2.1.6

For a complete list of all IVI drivers from Keysight, please visit www.keysight.com/find/drivers

Keysight modular drivers also require that Keysight IO Libraries Suite 16.0 or greater be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite

Version Details
  Current Version Previous Version
Version 1.2.1.6 1.1.1
Models Supported M9502A, M9505A M9502A, M9505A
IO Libraries Required Version

1.6.2

16.0 Update 1
Driver Types and Version IVI-C (32/64-bit) 1.2.1.6
IVI-COM (32/64-bit) 1.2.1.6
LabVIEW (32/64-bit) 1.2.1.6
MATLAB (32-bit) 1.2.1.6
IVI-C (32/64-bit) 1.1.1.1
IVI-COM (32/64-bit) 1.1.1.1
LabVIEW (32/64-bit) 1.1.1.1
MATLAB (32-bit) 1.1.1.1
Soft Front Panel Version 1.2.1.6 1.1.1.1
IVI Classes Supported 1.0 IVIDriver 1.0
Minimum IVI Shared Components Version 2.1.1 2.1.1
Version History • Increased the chassis fan speed (requires chassis firmware version 1.3.23 or later).
• Added support for Keysight IO Libraries 16.2.
• On 64-bit systems, the Keysight IO Libraries version 16.2 32-bit mDNS responder patch is installed automatically.
Initial Release


 

是德建议使用最新的版本,其中包括最新的漏洞修复和安全补丁
发布日期 版本 版本说明
2020-04-15 1.4.4.1 See above.
发布日期 版本
2020-04-15 1.4.4.1
版本说明
See above.

Driver 1.4.4.1 fixes the issues below:

  • Repair an enumeration and detection issue where the chassis cannot be detected in Keysight IO Libraries.
  • This driver with combination of chassis firmware 1.3.44 together would repair an intermittent issue where the chassis is unable to communicate with modules after a boot up.

 

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), Labview (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

安装到: PC

操作系统

  • Windows 7
  • Windows 8.1
  • Windows 10

支持的仪器

  • M9502A, M9505A

驱动程序类型:IVI-C(32 位/64 位)、IVI-COM(32 位/64 位)、Labview(32 位/64 位)、MATLAB(仅限 32 位)
 

IVI 类型支持:IviDriver 1.0

如何下载

  1. 单击 “下载” 按钮。
  2. 选择适当的可执行文件。
  3. 选择 “运行”。

如何安装

  • 运行下载的安装程序。

颁发许可证

  • 不要求具有许可证

安装到: PC

操作系统

  • Windows 7
  • Windows 8.1
  • Windows 10

支持的仪器

  • M9502A, M9505A

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), Labview (32-bit/64-bit), MATLAB (32-bit only)
 

IVI class support: IviDriver 1.0

如何下载

  1. Click the Download button.
     
  2. Select the appropriate executable file.
     
  3. Choose Run.

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

安装到: PC

操作系统

  • Windows 8
  • Windows 7
  • Windows XP

前提要求

支持的仪器

  • M9502A, M9505A

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

安装到: PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

支持的仪器

  • M9502A, M95905A

如何下载

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run

如何安装

  • See Documentation

颁发许可证

  • 不要求具有许可证

安装到: PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

支持的仪器

  • M9502A M9505A
SHOW MORE