您希望搜索哪方面的内容?
532xx 频率计数器 IVI 仪器驱动程序
For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers
This driver download installs the IVI-C, IVI-COM, and MATLAB driver components.
Keysight instrument drivers also require that Keysight IO Libraries Suite be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite
Current Version Details | |
---|---|
Version | 1.0.6.0 |
Models Supported | 53210A, 53220A, 53230A |
IO Libraries Required Version | 16.0 or greater |
IVI Classes Supported | IviCounter 1.0 (IVI-COM only) IviDriver 1.0 |
Minimum IVI Shared Components Version | 2.1.1.0 |
发布日期 | 版本 | 版本说明 |
---|---|---|
2017-02-04 | 1.2.2.0 | See Version Description above. |
发布日期 | 版本 |
---|---|
2017-02-04 | 1.2.2.0 |
版本说明 |
---|
See Version Description above. |
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0, IviCounter 2.0
Version Description: Updated the implementation of the Counter class’s Pulse width configure method to use the value of channel slope to change the polarity while doing the measurement and updated the implementation of IviCounter.PulseWidth.Configure method to use the Estimate value as provided by the user instead of default value.
如何下载
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
如何安装
Run the downloaded Installer.
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 8
- Windows 7
- Windows 10
前提要求
支持的仪器
- 53210A, 53220A, 53230A
相关链接
如何下载
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
如何安装
Run the downloaded installer.
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- 53210A, 53220A, 53230A
相关链接
如何下载
- 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run.
如何安装
- See Readme File
颁发许可证
- 不要求具有许可证
支持文档
下载
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- 53210A, 53220A, 53230A