The instrument driver provides access to the functionality of the Keysight V2920A through a COM server or C API which also complies with the IVI specifications. This driver works in any development environment which supports COM programming including Microsoft® Visual Basic, Microsoft Visual C++, Microsoft .NET, Keysight VEE Pro, National Instruments LabView, National Instruments LabWindows, and others.

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2010-04-10 5.0.4.0 The instrument driver provides access to the functionality of the Keysight V2920A through a COM server or C API which also complies with the IVI specifications.
Veröffentlichungsdatum Version
2010-04-10 5.0.4.0
Version Description
The instrument driver provides access to the functionality of the Keysight V2920A through a COM server or C API which also complies with the IVI specifications.

How to Download

  • Click the Download button. Select the appropriate executable file. Choose Run.

How to Install

  • See Documentation

Lizenzierung

  • Does Not Require a License

Supporting Documentation

Installs on: PC

Operating System

  • Windows Vista
  • Windows XP
  • Windows 2000

Voraussetzungen

  • See Documentation

Supported Instruments

  • V2920A
Keine Softwareversion verfügbar
SHOW MORE