For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

Keysight IVI drivers also require the Keysight IO Libraries Suite to be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite

Current Version Details
Version 1.0.4.0
Models Supported 4356A, 6641A, 6642A, 6643A, 6644A, 6645A, 6651A, 6652A, 6653A, 6654A, 6655A, 6671A, 6672A, 6673A, 6674A, 6675A, 6680A, 6681A, 6682A, 6683A, 6684A, 6690A, 6691A, 6692A
Driver Type IVI-COM
IVI Classes Supported IviDCPwr 2.0 IVI-COM
IviDriver 1.0 IVI-COM
IVI-COM ProgID Keysight66xx.Keysight66xx
Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2003-05-07 1.0.4.0 IVI-COM Version 1.0.4.0 for 66xx Power Supply Modules
Release Date Version
2003-05-07 1.0.4.0
Version Description
IVI-COM Version 1.0.4.0 for 66xx Power Supply Modules

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  1. Install both pre-requesites first
  2. Install the driver

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Supported Instruments

  • 6641A 6645A, 6651A 6655A, 6671A 6675A, 6680A 6684A, 6690A 6692A, E4356A

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  1. Install both pre-requesites first
  2. Run the downloaded installer

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP

Supported Instruments

  • 6641A 6645A, 6651A 6655A, 6671A 6675A, 6680A 6684A, 6690A 6692A, E4356A
SHOW MORE