Software Release Date: Jan, 2009
Software Requirement: Keysight TestExec SL 6.1.1

This patch is ONLY applicable to 6.1.1 version. Please ensure you are having TestExec 6.1.1 version before installing

To install the TestExec SL 6.1.1 Hotfix61101 Patch:

Click on "TestExec SL 6.1.1 Hotfix61101 Patch" Download. Save this file to disk.

  1. Extract the files to a temporary folder
  2. Copy the files "utacore.dll" and "utacore.pdb" from the temporary folder to folder "\Program Files\Keysight\TestExec SL 6.1\Bin".
  3. Overwrite the existing files.
  4. Remove the temporary folder
Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2009-01-08 6.1.1 Hotfix 61101 This patch is ONLY applicable to 6.1.1 version. It will fix the service manager local host error during the first run of the testplan when calling the action of Keysight VEE Pro 8.5 or above.
Veröffentlichungsdatum Version
2009-01-08 6.1.1 Hotfix 61101
Version Description
This patch is ONLY applicable to 6.1.1 version. It will fix the service manager local host error during the first run of the testplan when calling the action of Keysight VEE Pro 8.5 or above.

How to Download

  • See Above

How to Install

  • See Above

Lizenzierung

  • Does Not Require a License

Supporting Documentation

Installs on: PC

Voraussetzungen

  • See Readme File
Keine Softwareversion verfügbar
SHOW MORE