Software Release Date: Jan, 2009
Software Requirement: Keysight TestExec SL 6.1.1

This patch is ONLY applicable to 6.1.1 version. Please ensure you are having TestExec 6.1.1 version before installing

To install the TestExec SL 6.1.1 Hotfix61101 Patch:

Click on "TestExec SL 6.1.1 Hotfix61101 Patch" Download. Save this file to disk.

  1. Extract the files to a temporary folder
  2. Copy the files "utacore.dll" and "utacore.pdb" from the temporary folder to folder "\Program Files\Keysight\TestExec SL 6.1\Bin".
  3. Overwrite the existing files.
  4. Remove the temporary folder
是德建議使用最新的版本,其中包括最新的漏洞修復與安全覆蓋
發佈日期 版本 版本說明
2009-01-08 6.1.1 Hotfix 61101 This patch is ONLY applicable to 6.1.1 version. It will fix the service manager local host error during the first run of the testplan when calling the action of Keysight VEE Pro 8.5 or above.
發佈日期 版本
2009-01-08 6.1.1 Hotfix 61101
Version Description
This patch is ONLY applicable to 6.1.1 version. It will fix the service manager local host error during the first run of the testplan when calling the action of Keysight VEE Pro 8.5 or above.

如何下載

  • See Above

如何安裝

  • See Above

授權

  • Does Not Require a License

支援文件

Installs on: PC

參加條件

  • See Readme File
無可用的軟體版本
SHOW MORE