您希望搜索哪方面的内容?
34980A 多功能开关/测量主机和模块 IVI 仪器驱动程序
For a complete list of all IVI drivers from Keysight, please visit IVI-COM and IVI-C Drivers
Keysight IVI drivers also require the Keysight IO Libraries Suite to be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite
Current Version Details | |
---|---|
Version | 1.4.2.0 |
Models Supported | 34980A and modules 34921A, 34922A, 34923A, 34924A, 34925A, 34931A, 34932A, 34933A, 34934A, 34937A, 34938A, 34939A, 34941A, 34942A, 34945A, 34946A, 34947A, 34950A, 34951A, 34952A, 34959A |
Driver Type | IVI-COM and IVI-C |
IVI Classes Supported | IviDmm 3.0 IVI-COM IviDriver 1.0 IVI-C IviDriver 1.0 IVI-COM IviSwtch 3.0 IVI-C IviSwtch 3.0 IVI-COM |
IVI-C Prefix | Ag34980a ag34945A ag34951a ag34952a ag34959A |
IVI-COM ProgID | Keysight34980A.Keysight34980A Keysight34945A.Keysight34945A Keysight34950A.Keysight34950A Keysight34952A.Keysight34952A Keysight34959A.Keysight34959A |
.NET Namespace | |
Minimum IVI Shared Components Version | |
Driver Download | See links below. |
Readme Download | See links below. |
Help File Download (.chm) |
Special Note
The standard driver and the NI Switch Executive version have been combined into a single driver starting with revision 1.4.2.0 of the driver.
发布日期 | 版本 | 版本说明 |
---|---|---|
2022-12-12 | 1.6.0.0 | Defect fix |
发布日期 | 版本 |
---|---|
2022-12-12 | 1.6.0.0 |
版本说明 |
---|
Defect fix |
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0, IviDmm 4.1 (IVI-COM only), IviSwtch 4.0 - the following modules are not supported by the IviSwtch API: 34945A, 34950A, 34951A, 34952A, 34959A
如何下载
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
如何安装
Run the downloaded installer.
颁发许可证
- Does Not Require a License
支持文档
Installs on: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
- Windows 10
前提要求
支持的仪器
- Frame: 34980A Modules: 34921A, 34922A, 32923A, 34924A, 34925A, 34931A, 34932A, 34933A, 34934A, 34937A, 34938A, 34939A, 34941A, 34942A, 34945A, 34946A, 34947A, 34950A, 34951A, 34952A, 34959A
相关链接
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0, IviDmm 4.1 (IVI-COM only), IviSwtch 4.0 - the following modules are not supported by the IviSwtch API: 34945A, 34950A, 34951A, 34952A, 34959A
如何下载
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
如何安装
Run the downloaded installer.
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
- Windows 10
前提要求
支持的仪器
- Frame: 34980A Modules: 34921A, 34922A, 32923A, 34924A, 34925A, 34931A, 34932A, 34933A, 34934A, 34937A, 34938A, 34939A, 34941A, 34942A, 34945A, 34946A, 34947A, 34950A, 34951A, 34952A, 34959A
相关链接
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0, IviDmm 4.1 (IVI-COM only), IviSwtch 4.0 - the following modules are not supported by the IviSwtch API: 34945A, 34950A, 34951A, 34952A, 34959A
如何下载
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
如何安装
Run the downloaded installer.
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- Frame: 34980A Modules: 34921A, 34922A, 32923A, 34924A, 34925A, 34931A, 34932A, 34933A, 34934A, 34937A, 34938A, 34939A, 34941A, 34942A, 34945A, 34946A, 34947A, 34950A, 34951A, 34952A, 34959A
相关链接
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)
IVI class support: IviDriver 1.0, IviDmm 4.1 (IVI-COM only), IviSwtch 4.0 - the following modules are not supported by the IviSwtch API: 34945A, 34950A, 34951A, 34952A, 34959A
如何下载
- Click the Download button.
- Select the appropriate executable file.
-
Choose Run.
如何安装
Run the downloaded installer.
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- Frame: 34980A Modules: 34921A, 34922A, 32923A, 34924A, 34925A, 34931A, 34932A, 34933A, 34934A, 34937A, 34938A, 34939A, 34941A, 34942A, 34945A, 34946A, 34947A, 34950A, 34951A, 34952A, 34959A
相关链接
Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)
IVI class support: IviDriver 1.0, IviDmm 4.1 (IVI-COM only), IviSwtch 4.0 - the following modules are not supported by the IviSwtch API: 34945A, 34950A, 34951A, 34952A, 34959A
如何下载
- Click the Download button.
- Select the appropriate executable file.
-
Choose Run.
如何安装
Run the downloaded installer.
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
IVI Shared Components 2.2.1.0 or later from www.ivifoundation.org
支持的仪器
- Frame: 34980A Modules: 34921A, 34922A, 32923A, 34924A, 34925A, 34931A, 34932A, 34933A, 34934A, 34937A, 34938A, 34939A, 34941A, 34942A, 34945A, 34946A, 34947A, 34950A, 34951A, 34952A, 34959A
相关链接
如何下载
- Click the Download button.
- Select the appropriate executable file.
- Choose Run.
如何安装
Run the downloaded installer.
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- Frame 34980A Module 34921A 34922A 34923A 34924A 34925A 34931A 34932A 34933A 34934A 34937A 34938A 34939A 34941A 34942A 34945A 34946A 34947A 34950A 34951A 34952A 34959A
相关链接
如何下载
- Click the Download button. Select the appropriate executable file. Choose Run.
如何安装
- See Documentation
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- Frame 34980A Module 34921A 34922A 34923A 34924A 34925A 34931A 34932A 34933A 34934A 34937A 34938A 34939A 34941A 34942A 34945A 34946A 34947A 34950A 34951A 34952A 34959A
相关链接
如何下载
- Click the Download button. Select the appropriate executable file. Choose Run.
如何安装
- See Documentation
颁发许可证
- 不要求具有许可证
支持文档
下载
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- Frame 34980A Module 34921A 34922A 34923A 34924A 34925A 34931A 34932A 34933A 34937A 34938A 34941A 34942A 34945A 34946A 34947A 34950A 34951A 34952A 34959A
相关链接
如何下载
- Click the Download button. Select the appropriate executable file. Choose Run.
如何安装
- See Documentation
颁发许可证
- 不要求具有许可证
支持文档
下载
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- Frame 34980A Module 34921A 34922A 34923A 34924A 34925A 34931A 34932A 34933A 34937A 34938A 34941A 34942A 34945A 34946A 34947A 34950A 34951A 34952A 34959A
相关链接
如何下载
- Click the Download button. Select the appropriate executable file. Choose Run.
如何安装
- See Documentation
颁发许可证
- 不要求具有许可证
支持文档
下载
安装到: PC
操作系统
- Windows 7
- Windows Vista
- Windows XP
前提要求
支持的仪器
- Frame 34980A Module 34921A 34922A 34923A 34924A 34925A 34931A 34932A 34933A 34937A 34938A 34941A 34942A 34945A 34946A 34947A 34950A 34951A 34952A 34959A